990-91460C-001

Installation Procedure for Galaxy VL UPS with Bottom Entry Cabinet

NOTE: All power cables and signal cables can be routed through the bottom entry cabinet and connected in the UPS.
  1. Install the Seismic Anchoring with the Galaxy VL UPS (Option).
  2. Perform one of the following:
  3. Follow the UPS installation manual to connect the power cables and the signal cables and to complete the rest of the UPS installation.
For moving or decommissioning the bottom entry cabinet after installation has been completed, see Decommission or Move the Bottom Entry Cabinet to a New Location.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.