Decommission or Move the Bottom Entry Cabinet to a New Location
- Shut down the UPS completely – follow the instructions in the UPS operation manual.
- Lockout/Tagout all breakers in the switchgear in the OFF (open) position.
- Lockout/Tagout all battery breakers in the switchgear/battery solution in the OFF (open) position.
- Perform the following for the UPS. See the UPS installation
manual for details.
- Measure for and verify ABSENCE of voltage on each input/bypass/output/DC
busbar in the UPS before continuing.
DANGER hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHMeasure for and verify ABSENCE of voltage on each input/bypass/output/DC busbar before continuing.Failure to follow these instructions will result in death or serious injury. - Disconnect all power cables from the UPS.
- Disconnect and remove any signal cables from the UPS.
- Measure for and verify ABSENCE of voltage on each input/bypass/output/DC
busbar in the UPS before continuing.
- Perform the following for the bottom entry cabinet. See Install the Bottom Entry Cabinet with the Galaxy VL UPS in
System over 45 kAIC/kA Icw, Install the Bottom Entry Cabinet with the Galaxy VL UPS in
System up to 45 kAIC/kA Icw, or Install the Bottom Entry Cabinet with the Easy UPS 3L for details.
- Remove the power cables from the bottom entry cabinet.
- Remove the signal cables from the bottom entry cabinet.
- Remove the interconnection hardware between the UPS and the bottom entry cabinet.
- If present, remove the seismic front anchoring bracket.
- Raise the feet of the bottom entry cabinet until the casters have full contact with the floor.
- You can now move the bottom entry cabinet by rolling it
over the floor on the casters.
WARNING TIPPING hazard- The casters of the bottom entry cabinet are exclusively for transport on flat, even, hard, and horizontal surfaces.
- The casters of the bottom entry cabinet are intended for transport over short distances (i.e. inside the same building).
- Move at a slow pace and pay close attention on the floor conditions and the balance of the bottom entry cabinet.
Failure to follow these instructions can result in death, serious injury, or equipment damage. - If present, remove the rear seismic anchoring bracket from the bottom entry cabinet and remove the seismic anchors from the floor. Save for reinstallation.
- For transport over longer distances or in conditions
that are not suitable for the casters of the bottom entry cabinet:
WARNING TIPPING hazardFor transport over longer distances or in conditions that are not suitable for the casters of the bottom entry cabinet, ensure:- that personnel performing the transport have necessary skill and have received adequate training;
- to use appropriate tools to safely lift and transport the bottom entry cabinet;
- to protect the product against damage by using appropriate protection (like wrapping or packaging).
Failure to follow these instructions can result in death, serious injury, or equipment damage.Transportation requirements:
-
Mount the bottom entry cabinet in a vertical position in the center of a suitable pallet with minimum pallet dimensions: 800 mm x 800 mm (31.5 in x 31.5 in)). The pallet must be suitable for the weight of the bottom entry cabinet, which weighs 85 kg (188 lbs).
-
Use appropriate means of fixation to mount the bottom entry cabinet to the pallet.
-
The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.
DANGER TIPPING hazard- The bottom entry cabinet must be appropriately fixed to the pallet immediately after being placed on the pallet.
- The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
Failure to follow these instructions will result in death or serious injury.WARNING Unexpected equipment behaviorDo not lift the bottom entry cabinet with a forklift/pallet truck directly on the frame as it may bend or damage the frame.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Perform one of the following:
- Decommission the bottom entry cabinet, OR
- Move the bottom entry cabinet to a new location to install it.
- Only for installing the bottom entry cabinet in a new
location: Follow the installation manual to install the bottom
entry cabinet in the new location. See Installation Procedure for Galaxy VL UPS with Bottom Entry
Cabinet or Installation Procedure for Easy UPS 3L with Bottom Entry Cabinet for installation overview. Startup must only be performed
by Schneider Electric.
DANGER hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHStartup must only be performed by Schneider Electric.Failure to follow these instructions will result in death or serious injury.