990-91735-001

Environment

  Operating Storage
Temperature 0 °C to 40 °C (32 °F to 122 °F) -20 °C to 60°C (-4 °F to 140 °F)
Relative humidity 10-90% non-condensing
Elevation Designed for operation in 0-2000 m (0-6600 feet)
Protection class IP20
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?