990-91735-001

Torque Specifications

Bolt size Torque
M6 9 Nm (6.64 lb-ft)
M8 17 Nm (12.54 lb-ft)
Input / output terminals 0.6 Nm (0.44 lb-ft)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?