990-91735-001

View the Active Alarms

When there is an active alarm in the system, a symbol indicating the alarm level is shown in the top right corner of the screen and the buzzer is active.

  1. Tap the alarm status symbol to access the active alarms log. The log shows the latest 100 events with the newest events at the top of the list.
    1. Tap the arrow buttons to scroll up and down.
    2. Tap Severity, Date,Time or UPS #ID to sort the events.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?