990-94382A-001

Connect the Power Cables in the I/O Cabinet

Hardware is provided in installation kit TME67411 for this procedure.

DANGER
Hazard of electric shock, explosion, or arc flash
  • Only use the provided bolts to connect the power cables to the busbars in the I/O cabinet.
  • Use the correct bolt size and length as described.
Failure to follow these instructions will result in death or serious injury.
  1. Route the power cables through the top of the I/O cabinet.
  2. Connect the EGC cable to the ground busbar. Use the provided M12x45mm bolts.
  3. Connect the neutral cables to the N busbar. Use the provided M12x45mm bolts.
  4. Connect the DC cables to the DC busbars (DC+, DC-). Use the provided M12x55mm bolts.
  5. Connect the input cables to the input busbars (L1, L2, L3). Use the provided M12x45mm bolts.
  6. Connect the output cables to the output busbars (L1, L2, L3). Use the provided M12x45mm bolts.
  7. Close the inner door and fasten with the two screws. Reinstall the inner front lexan plates.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?