990-94382A-001

Final installation

  1. Reinstall the front plates on the I/O cabinet.

    Front View

  2. Reinstall the cover over the signal connections on UPS 1-4.

    Front View

  3. Install the front transportation brackets on the UPSs – the front transportation brackets were removed during unpacking. Reinstall the front anchoring bracket on the I/O cabinet, if it has been removed during unpacking.
    NOTICE
    Risk of equipment damage
    Install the front transportation brackets to avoid the UPS and I/O cabinet overheating from circulating hot air from the rear outlets. The front transportation brackets block the hot air backflow.
    Failure to follow these instructions can result in equipment damage.
  4. Only for seismic anchoring: Mount the front anchoring brackets on all the cabinets to the floor.
  5. Close the front door(s) and lock the handle with the provided key.
  6. Only for seismic anchoring: Install the provided seismic top brackets on the cabinets using the provided M6x16 flat screws (803-9562).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?