990-94382A-001

Interconnect the Cabinets

  1. Lower the front leveling feet of the cabinets with a wrench until they connect with the floor. Use a bubble-leveler to check that the cabinets are level.
    NOTICE
    Risk of equipment damage
    Do not move the cabinets after the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.
  2. Interconnect the cabinets in the front with screws as shown.
  3. Interconnect the cabinets in the front with four brackets as shown.
  4. Remove the top gland plates from the I/O cabinet.
  5. Drill/punch holes for power cables or conduits in the gland plates from the I/O cabinet. Install conduits (not provided), if applicable.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the cabinet.
    Failure to follow these instructions will result in death or serious injury.
  6. Reinstall the top gland plates on the I/O cabinet.
  7. Interconnect the cabinets in the top with the four provided brackets and the provided M6x16 flat screws (803-9562).
  8. Interconnect the cabinets in the top rear with the four provided brackets and the existing M6x16 flat screws (803-9562).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?