990-94382A-001

Installation Procedure

TIP: The cabinets are very tall. Use appropriate equipment to get adequate working access to the top of the cabinets like mobile ladders with platforms, raised podiums, or similar.
  1. Prepare the Cabinets for Installation.
  2. Install the Seismic Anchoring and Position the Cabinets.
  3. Interconnect the Cabinets.
  4. Connect the Power Cables in the I/O Cabinet.
  5. For UPS 1-4: Install the ERMS Door Switch Kit GVLOPT011.
  6. Connect the Internal Signal Cables Between the UPSs and the I/O Cabinet.
  7. For UPS 1-4: Connect the Signal Cables.
  8. For UPS 1-4: Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products.
  9. For UPS 1-4: Connect the External Communication Cables.
  10. For UPS 1-4: Connect the Modbus Cables.
  11. For UPS 1-4: Install the Power Module(s).
  12. Final installation.
For moving or decommissioning the UPS system after installation has been completed, please see Decommission or Move the UPS System to a New Location.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?