990-91379E-001

Operation Modes

The UPS has two different levels of operation modes:

  • UPS mode: The operation mode of the individual UPS. See UPS Modes.

  • System mode: The operation mode of the complete UPS system that supplies the load. See System Modes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?