990-91379H-001

Configure the Network

The network can be configured for the integrated and the optional network management card (NMC).

  1. Tap Configuration > Network and select IPv4 for the Integrated NMC to configure the integrated network management card or for the Optional NMC to configure the optional network management card (if present).
  2. Configure the IPv4 settings on the page for the chosen NMC:
    1. Remove the check mark for Disable integrated NMC IPv4/Disable optional NMC IPv4 to configure the IPv4. When the check mark is present, no settings can be made and the function is disabled.
    2. Set the Address mode to Manual, DHCP, or BOOTP. For manual address mode, add the values.
    3. Tap OK to save your settings.
  3. Tap Configuration > Network and select IPV6 for the Integrated NMC to configure the integrated network management card or for the Optional NMC to configure the optional network management card (if present).
  4. Configure the IPv6 settings on the page for the chosen NMC:
    1. Remove the check mark for Disable integrated NMC IPv6/Disable optional NMC IPv6 to configure the IPv6. When the check mark is present, no settings can be made and the function is disabled.
    2. Set the DHCPV6 mode to Address and other information, Non-address information only, or IPv6 never.
    3. Select Auto configuration or Manual. For manual mode, add the values.
    4. Tap OK to save your settings.
  5. Repeat the steps to configure the other NMC, if needed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.