990-91379H-001

View Configuration for Prioritizing Battery Operation When Input Contact is Activated

The feature Prioritize battery operation when input contact is activated allows you to prioritize battery operation to remove your load from the grid at certain times/in certain situations, controlled by an input contact signal. When this feature is enabled, the UPS will transfer to battery operation on an input contact signal. When the input contact signal is deactivated, the UPS will return to its default operation mode. It is also possible to set a specified time limit (maximum 120 seconds) that the UPS is allowed to stay in battery operation. When the specified time limit is over, the UPS will return to its default operation mode even though the input contact signal is still activated.
The UPS will only transfer to battery operation if battery operation is possible, i.e. if there is sufficient runtime available from the batteries and no other restrictions are detected. Enabling this feature and setting the time limit for battery operation are only configurable by Schneider Electric Service.

  1. Tap Configuration > Grid interactive UPS to see if Prioritize battery operation when input contact is activated is enabled/disabled.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?