990-91216D-001

Connect the Power Cables on GVSBPAR60K120H for a 3:3 UPS System

  1. Connect the PE cables to the PE busbar.
  2. Connect the input cables/bypass cables from utility/mains.
  3. Connect the UPS input cables/UPS bypass cables from UPS 1.
  4. Connect the UPS input cables/UPS bypass cables from UPS 2.
  5. Connect the UPS output cables from UPS 1.
  6. Connect the UPS output cables from UPS 2.
  7. Connect the load cables.
  8. Fasten the cables with cable ties (provided) to the cable reliefs as shown.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.