990-91216D-001

Remove the Neutral Jumper

NOTE: The neutral jumper makes a bolted connection of the neutral so that the neutral is not disconnected when the 4-pole breakers are opened.
NOTE: Only remove the neutral jumpers in a Galaxy VS installation, if this is a local requirement. Removal of the neutral jumpers is an option for a Galaxy VS installation.
NOTE: Always remove the neutral jumpers in an Easy UPS 3S installation and in an Easy UPS 3M installation. Removal of the neutral jumpers is mandatory for an Easy UPS 3S installation and for an Easy UPS 3M installation.
  1. Remove the neutral jumpers (cable and/or busbar) between UOB1 and UOB2. Reinstall the screws in the same position.
  2. Remove the neutral jumpers on the MBB (cable or busbar).

    GVSBPAR10K30H

    GVSBPAR40K50H

    GVSBPAR60K120H

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.