990-91216D-001

Decommission or Move the Parallel Maintenance Bypass Panel to a New Location

  1. Shut down the UPS completely – follow the instructions in the UPS operation manual.
  2. Lockout/Tagout all breakers in the switchgear in the OFF (open) position.
  3. Lockout/Tagout all battery breakers in the switchgear/battery solution in the OFF (open) position.
  4. Verify that all upstream breakers are in the OFF (open) position.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    Verify that all upstream breakers are in the OFF (open) position.
    Failure to follow these instructions will result in death or serious injury.
  5. Open the front door of the parallel maintenance bypass panel.
  6. Lockout/Tagout UIB1, UIB2, UOB1, UOB2, and MBB in the parallel maintenance bypass panel in the OFF (open) position.
  7. Remove the screws and open the inner door in the parallel maintenance bypass panel.
  8. Measure for and verify ABSENCE of voltage on each input/bypass busbar, UPS input/UPS bypass busbar, UPS output busbar, and load busbar before continuing.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Measure for and verify ABSENCE of voltage on each input/bypass busbar, UPS input/UPS bypass busbar, UPS output busbar, and load busbar before continuing.
    Failure to follow these instructions will result in death or serious injury.

    GVSBPAR10K30H

    GVSBPAR40K50H

    GVSBPAR60K120H

  9. Disconnect and remove all power cables from the parallel maintenance bypass panel. See Connect the Power Cables on GVSBPAR10K30H, Connect the Power Cables on GVSBPAR40K50H for a 3:1 UPS System, Connect the Power Cables on GVSBPAR40K50H for a 3:3 UPS System, Connect the Power Cables on GVSBPAR60K120H for a 3:1 UPS System, or Connect the Power Cables on GVSBPAR60K120H for a 3:3 UPS System for details.
  10. Disconnect and remove all signal cables from the parallel maintenance bypass panel. See Connect the Signal Cables for Galaxy VS UPSs, or Connect the Signal Cables for Easy UPS 3S and Easy UPS 3M for details.
  11. Remove the four screws from the wall and remove the parallel maintenance bypass panel from the wall.
    CAUTION
    Heavy load
    GVSBPAR10K30H weighs 35 kg, GVSBPAR40K50H weighs 86 kg, and GVSBPAR60K120H weighs 110 kg. Use appropriate tools to safely lift the parallel maintenance bypass panel.
    Failure to follow these instructions can result in injury or equipment damage.
  12. Close the inner door and fasten it with the screws.
  13. Close and lock the front door of the parallel maintenance bypass panel.
  14. For transport:
    WARNING
    TIPPING hazard
    For transport of the parallel maintenance bypass panel ensure:
    • that personnel performing the transport have necessary skills and have received adequate training;
    • to use appropriate tools to safely lift and transport the product;
    • to protect the product against damage by using appropriate protection (like wrapping or packaging).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Transportation requirements:

    • Mount the parallel maintenance bypass panel in a horizontal position in the center of a suitable pallet with minimum pallet dimensions: 1000 mm x 1200 mm. The pallet must be suitable for the weight of the parallel maintenance bypass panel (35-110 kg).

    • Mount the parallel maintenance bypass panel to the pallet with appropriate means of fixation that can withstand vibrations and shocks during loading, transport, and unloading.

    • The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.

    WARNING
    Unexpected equipment behavior
    Do not lift the parallel maintenance bypass panel with a forklift/pallet truck directly as it may bend or damage the parallel maintenance bypass panel.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  15. Perform one of the following:
    • Decommission the parallel maintenance bypass panel, OR
    • Move the parallel maintenance bypass panel to a new location to install it.
  16. Only for installing the parallel maintenance bypass panel in a new location: Follow the installation manual to install the parallel maintenance bypass panel in the new location. See Installation Procedure for Galaxy VS or Installation Procedure for Easy UPS 3S and Easy UPS 3M for installation overview. Reinstallation and startup must only be performed by qualified personnel.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.