990-91263A-001

Interconnect Modular Battery Cabinet 1 and the Adjacent UPS with Internal Batteries

  1. Push modular battery cabinet 1 and the UPS into place.
  2. Install the three interconnection brackets between modular battery cabinet 1 and the UPS.
  3. Install the three interconnection screws between modular battery cabinet 1 and the UPS.
  4. Push the baying cover down between modular battery cabinet 1 and the UPS.

    Modular Battery Cabinet 1 and the UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?