990-91263A-001

Prepare Modular Battery Cabinet 1 for Signal Cables

  1. Remove the gland plates and the brush plates from the rear of modular battery cabinet 1.

    Rear View of Modular Battery Cabinet 1

  2. Perform one of the following:
    • For installation without conduits: Reinstall the brush plates.
    • For installation with conduits: Drill a hole in the gland plates for conduits, install conduits, and reinstall the gland plates.

    Rear View of Modular Battery Cabinet 1 without Conduits

    Rear View of Modular Battery Cabinet 1 with Conduits

  3. Route the Class 2/SELV signal cable through the left gland plate and into modular battery cabinet 1.
  4. Route the non-Class 2/non-SELV signal cable through the right gland plate and into modular battery cabinet 1.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.