990-91263A-001

Install the Conduit Box on the Modular Battery Cabinet

In an installation with a remote UPS rated for maximum 50 kW: Perform the steps below on modular battery cabinet 1.

In an installation with a remote UPS rated over 50 kW: Perform the steps below on all the modular battery cabinets.

  1. Remove the conduit box from the modular battery cabinet.

    Rear View of the Modular Battery Cabinet

  2. Remove the top or bottom gland plate from the conduit box.
  3. Drill/punch holes for power cables/conduits in the top or bottom gland plate. Install conduits (not provided), if applicable.
    DANGER
    hazard of electric shock, explosion, or arc flash
    Do not drill or punch holes with the gland plates installed and do not drill or punch holes in close proximity to the cabinet.
    Failure to follow these instructions will result in death or serious injury.
  4. Reinstall the top or bottom gland plate on the conduit box.
  5. Install the conduit box on the modular battery cabinet(s). Note that the conduit box is installed in the reverse position.

    Rear View of the Modular Battery Cabinet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.