990-91317G-006

Corriente residual

Instalación de sistema SAI 380/400/415 V de 4 cables a plena carga

Potencia nominal del SAI Corriente residual
20-50 kW 62 mA
Comentarios
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.