990-91262E-001

Parallel System Overview

UIB Unit input disconnect device
SSIB Static switch input disconnect device
IMB Internal maintenance disconnect device
UOB Unit output disconnect device
SIB System isolation disconnect device
BB1 Battery disconnect device in UPS for internal batteries
BB2 Battery disconnect device in external battery solution (if present)
MBB Maintenance bypass disconnect device
NOTE: In Schneider Electric literature, 'disconnect device' is used as a generic term covering circuit breakers or switches as their position may vary depending on configuration. Details about the individual configuration are found in the electrical diagram and/or by reading the symbol on the front of each disconnect device.

Simplified 1+1 Parallel Systems

Galaxy VS can support 2 UPSs in a simplified 1+1 parallel system for redundancy with shared UIB and SSIB.

Simplified 1+1 Parallel System – Single Mains

Simplified 1+1 Parallel System – Dual Mains

Parallel Systems with Individual UIB and SSIB

Galaxy VS can support up to 4 UPSs in parallel for capacity and up to 3+1 UPSs in parallel for redundancy with individual UIB and SSIB.

NOTE: IMB can only be used in a simplified 1+1 parallel system. In any other parallel system, an external MBB must be provided and IMB* must be padlocked in the open position.

Parallel System – Single Mains

Parallel System – Dual Mains

Parallel Systems with Shared UIB and SSIB

Galaxy VS can support up to 4 UPSs in parallel for capacity and up to 3+1 UPSs in parallel for redundancy with shared UIB and SSIB.

NOTE: IMB can only be used in a simplified 1+1 parallel system. In any other parallel system, an external MBB must be provided and IMB* must be padlocked in the open position.

Parallel System – Single Mains

Parallel System – Dual Mains

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.