Decommission or Move the UPS to a New Location
- Shut down the UPS completely – follow the instructions in the UPS operation manual.
- Lockout/Tagout the battery disconnect device BB to the open (OFF) position on the UPS.
- Lockout/Tagout all disconnect devices in the maintenance bypass cabinet/maintenance bypass panel/maintenance bypass panel/switchgear in the OFF (open) position.
- Lockout/Tagout all battery disconnect devices in the switchgear/battery solution in the OFF (open) position.
- Open the front door of the UPS.
- Lockout/Tagout the internal maintenance disconnect device IMB in the OFF (open) position.
- Remove the power modules from the UPS:
CAUTIONHeavy loadPower modules are heavy and require two persons to lift.- 20 kW power module weighs 25 kg (55 lbs).
- 50 kW power module weighs 38 kg (84 lbs).
Failure to follow these instructions can result in injury or equipment damage.- Remove the screws and push the unlock switch.
- Pull the power module halfway out. A locking mechanism prevents the power module from being pulled all the way out.
- Release the lock by pressing the release button on both sides of the power module and remove the power module.
- Install a filler plate (if available) in front of the empty power module slot.
- Store the power modules safely until reinstallation.
WARNINGrisk of equipment damage- Store the power modules at an ambient temperature of -15 to 40 °C (5 to 104 °F), 10-80% non-condensing humidity.
- Store the power modules in their original protective packaging.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
- Remove the battery cover and the middle plate.
- Disconnect the battery terminals from the front of all
the battery modules.
DANGERHazard of electric shock, explosion, or arc flashBatteries can present a risk of electric shock and high short-circuit current. The following precautions must be observed when working on batteries:- Servicing of batteries must only be performed or supervised by qualified personnel knowledgeable of batteries and the required precautions. Keep unqualified personnel away from batteries.
- Do not dispose of batteries in a fire as they can explode.
- Do not open, alter, or mutilate batteries. Released electrolyte is harmful to the skin and eyes. It may be toxic.
- Remove watches, rings, or other metal objects.
- Use tools with insulated handles.
- Wear protective glasses, gloves and boots.
- Do not lay tools or metal parts on top of batteries.
- Set the battery disconnect device BB to the open (OFF) position before starting this procedure.
Failure to follow these instructions will result in death or serious injury. - Remove the battery modules from the three upper rows. Leave
the battery modules in the two bottom rows to increase weight stability.
CAUTIONHeavy loadBattery modules are heavy and require two persons to lift.- The battery module weighs 32 kg (71 lbs).
Failure to follow these instructions can result in injury or equipment damage.- Remove the screw from the battery module handle and turn the handle upwards.
- Pull the battery module carefully out of the slot.
- Store the battery modules correctly for reinstallation.
WARNINGrisk of equipment damage- If the UPS system remains de-energized for a long period, we recommend that you energize the UPS system for a period of 24 hours at least once every month. This charges the installed battery modules, thus avoiding irreversible damage from deep discharging.
- Store the battery modules at an ambient temperature of -15 to 40 °C (5 to 104 °F).
- Store the battery modules in their original protective packaging.
- Battery modules stored at -15 to 25 °C (5 to 77 °F) must be recharged every six months to avoid damages from deep discharging. Battery modules stored at over 25 °C (77 °F) must be recharged at shorter intervals.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
- Measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent cover for input, bypass, output, neutral, and DC.
- Remove the transparent cover.
- Measure for and verify ABSENCE of voltage on each input/bypass/output terminal before continuing.
- Disconnect and remove all power cables from the UPS. See Connect the Power Cables for details.
- For UPS system with adjacent modular battery cabinet: Disconnect and remove the DC extension busbars and the battery cables from the UPS. See Connect the Power Cables from an Adjacent Modular Battery Cabinet for details. Save the DC extension busbars and the battery cables for reinstallation.
- Remove the indicated covers.
- Disconnect and remove any signal cables from the front of the UPS. For UPS system with modular battery cabinet(s): See Connect the Signal Cables from a Modular Battery Cabinet for details. For simplified 1+1 parallel UPS system: See Connect the IMB Signal Cables in a Simplified 1+1 Parallel System for details.
- For UPS system with maintenance bypass cabinet: Remove the interconnection hardware between the UPS and the maintenance bypass cabinet. See the installation manual provided with the maintenance bypass cabinet for details. Save all parts for reinstallation.
- For UPS with system adjacent modular battery cabinet: Remove the interconnection hardware between the UPS and the adjacent battery cabinet. See the installation manual provided with the adjacent battery cabinet for details. Save all parts for reinstallation.
- Reinstall all removed plates and covers. Close and lock the front door.
- If present, remove the seismic front anchoring bracket from the UPS. Save for reinstallation.
- Raise the feet of the UPS until the casters have full contact with the floor.
- You can now move the UPS by rolling it over the floor on
the casters.
WARNINGTIPPING hazard- The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
- The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
- Move at a slow pace and pay close attention on the floor conditions and the balance of the UPS.
Failure to follow these instructions can result in death, serious injury, or equipment damage. - If present, remove the rear seismic anchoring bracket from the UPS and remove the seismic anchors from the floor. Save for reinstallation. See Install the Seismic Anchoring (Option) for details.
- For transport over longer distances or in conditions
that are not suitable for the casters of the UPS:
WARNINGTIPPING hazardFor transport over longer distances or in conditions that are not suitable for the casters of the UPS, ensure:- that personnel performing the transport have necessary skills and have received adequate training;
- to use appropriate tools to safely lift and transport the UPS;
- to protect the product against damage by using appropriate protection (like wrapping or packaging).
Failure to follow these instructions can result in death, serious injury, or equipment damage.Transportation requirements:
-
Mount the UPS in a vertical position in the center of a suitable pallet with minimum pallet dimensions: 805 mm x 1060 mm (32 in x 42 in)). The pallet must be suitable for the weight of the UPS (496 kg (1094 lbs) with no power modules and two bottom rows of battery modules present inside the UPS).
-
Use appropriate means of fixation to mount the UPS to the pallet.
-
The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.
DANGERTIPPING hazard- The UPS must be appropriately fixed to the pallet immediately after being placed on the pallet.
- The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
Failure to follow these instructions will result in death or serious injury.
WARNINGUnexpected equipment behaviorDo not lift the UPS with a forklift/pallet truck directly on the frame as it may bend or damage the frame.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Perform one of the following:
- Decommission the UPS, OR
- Move the UPS to a new location to install it.
- Only for installing the UPS in a new location: Follow
the installation manual to install UPS in the new location. See Installation Procedure for Single Systems or Installation Procedure for Parallel Systems for installation
overview. Startup must only be performed by Schneider Electric.
DANGERhAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASHStartup must only be performed by Schneider Electric.Failure to follow these instructions will result in death or serious injury.