990-91262E-001

Connect the Signal Cables from a Modular Battery Cabinet

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.
  1. Only for remote modular battery cabinet:
    1. Route the Class 2/SELV cables and non-Class 2/non-SELV cables into the UPS as shown.

      Class 2/SELV

      Non-Class 2/non-SELV

    2. Route the Class 2/SELV cables and non-Class 2/non-SELV cables to board 640-7552 in the UPS.

      Top View of the UPS

  2. Only for adjacent modular battery cabinet: Route the provided signal cables 0W76627 and 0W12908 to board 640-7552 in the UPS.

    Front View of Adjacent Modular Battery Cabinet 1 and the UPS

  3. Connect the signal cables from modular battery cabinet 1 to the UPS:
    1. Disconnect the termination plug from J8007 on board 640-7552 in the UPS.
    2. Mount the termination plug in J8007 on board 640-7572 in the last modular battery cabinet (T).
    3. Connect the signal cable from J8011 on board 640-7572 in modular battery cabinet 1 to J8014 on board 640-7552 in the UPS.
    4. Connect the signal cable from J8008 on board 640-7572 in modular battery cabinet 1 to J8007 on board 640-7552 in the UPS.
    Modular Battery Cabinet 2,3,4 Modular Battery Cabinet 1 UPS
  4. Reinstall the top plate on the UPS.
    1. Tilt the top plate and slide it onto the UPS from the rear. Taps in the rear of the top plate must connect to slots in the rear of the UPS.

      Rear View of the UPS

    2. Push the top plate down in the front and reinstall the screws.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.