990-91497C-001

Final Installation Steps

DANGER
hazard of electric shock, explosion, or arc flash
All panels and covers must be properly reinstalled prior to energizing the UPS.
Failure to follow these instructions will result in death or serious injury.
WARNING
Hazard of arc flash
  • Do not make mechanical changes to the product (including removal of cabinet parts or drilling/cutting of holes) that are not described in the installation manual.
  • The side panels of each individual cabinet must be installed in all installation types (including parallel installations with no air gap between the frames or in installations where the right-most cabinet and/or the left-most cabinet is placed against a wall). When the bypass inductor cabinet and the I/O cabinet are bayed together they will be considered as one cabinet and must have side panels installed on the left side and the right side.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Close the inner doors of the I/O cabinet and fasten the screws. Reinstall the front covers and the rear covers of the cabinets.
  2. Fasten the front anchoring brackets to the front of the cabinets.
  3. Mount the front anchoring brackets to the floor.
    NOTE: Floor anchoring bolts are not provided.
  4. Follow the UPS installation manual to complete the installation of the power cabinets and the I/O cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?