990-91497C-001

Position the Cabinets

DANGER
hazard of electric shock, explosion, or arc flash
Do not step/walk on top of the cabinets.
Failure to follow these instructions will result in death or serious injury.
NOTE: Rear access is required for interconnection of busbars between the bypass inductor cabinet and the I/O cabinet. If rear access is not available, complete the procedure described in Install Busbars between the Bypass Inductor Cabinet and the I/O Cabinet before pushing the cabinets into the final position (Step 5-8).
  1. Open the front door of the bypass inductor cabinet. Remove the front covers, the rear cover, and the plastic covers from the two cutouts on the right side.

    Front View of the Bypass Inductor Cabinet

  2. Remove the rear covers from the I/O cabinet.

    Front View of the I/O Cabinet

  3. Open the front doors and the three inner doors of the I/O cabinet.

    Front View of the Bypass Inductor Cabinet and the I/O Cabinet

  4. Remove the two rear bottom plates from the I/O cabinet.

    Front View of the I/O Cabinet

    NOTE: Rear access is required for interconnection of busbars between the bypass inductor cabinet and the I/O cabinet. If rear access is not available, complete the procedure described in Install Busbars between the Bypass Inductor Cabinet and the I/O Cabinet before pushing the cabinets into the final position (Step 5-8).
  5. Push the bypass inductor cabinet into position against the rear anchoring bracket – the cabinet will connect to the conic outcroppings on the rear anchoring bracket.

    Front View of the Bypass Inductor Cabinet

  6. Fasten the bypass inductor cabinet to the rear anchoring bracket by tightening the bolts on the front of the bypass inductor cabinet. Torque to 50 Nm (36.87 lb-ft).
  7. Push the I/O cabinet into position against the rear anchoring bracket - the I/O cabinet will connect to the conic outcroppings on the rear anchoring bracket.

    Front View of the I/O Cabinet

  8. Fasten the I/O cabinet to the rear anchoring bracket by tightening the bolts on the rear inside of the I/O cabinet. Torque to 50 Nm (36.87 lb-ft).
  9. Reinstall the two rear bottom plates in the I/O cabinet.
  10. Push the power cabinets one by one into position against the rear anchoring brackets – the cabinets will connect to the conic outcroppings on the brackets.
    CAUTION
    risk of equipment damage
    When pushing the power cabinet into position, push on the frame to avoid damaging the signal cables.
    Failure to follow these instructions can result in injury or equipment damage.
  11. Fasten the power cabinets to the rear anchoring brackets by tightening the bolts on the front of the power cabinets. Torque to 50 Nm (36.87 lb-ft).
  12. Lower the two front feet on all cabinets until they connect with the floor – use a bubble-leveler to ensure that the cabinets are level. Use the provided levelling shims if necessary.
  13. Install the top baying bracket from the installation kit 0H-9658 on the top of the bypass inductor cabinet and the I/O cabinet.

    Front View of the Bypass Inductor Cabinet and the I/O Cabinet

  14. Mount the M6 screws from the installation kit 0H-9658 from right to left in the marked positions between the I/O cabinet and the bypass inductor cabinet.

    From I/O Cabinet to Bypass Inductor Cabinet

  15. Mount the M6 screws from the installation kit 0H-9658 from right to left in the five marked positions between the power cabinets and in the four marked positions between the power cabinet and the I/O cabinet to interconnect the cabinets.

    From Power Cabinet to Power Cabinet

    From Power Cabinet to I/O Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?