990-91497C-001

Installation Procedure

  1. Remove the Cabinets from the Pallet.
  2. Mount the Rear Anchoring Brackets.
  3. Position the Cabinets.
  4. Prepare the I/O Cabinet for Internal Busbar Connection.
  5. Busbars will be connected by Schneider Electric during the assembly service.
  6. Prepare the I/O and Bypass Inductor Cabinet for Power Cables.
  7. Connect the Power Cables.
  8. Final Installation Steps.
  9. Follow the UPS installation manual to connect the output cables and DC cables in the I/O cabinet. Follow the procedure for a 480 V UPS system. Note that input cables and G are connected in the bypass inductor cabinet.
  10. Follow the UPS installation manual to complete the rest of the installation of the UPS system.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?