Mount the Rear Anchoring Brackets
![]() |
---|
hazard of electric shock, explosion, or arc flash
Leave the UPS system covered while making anchoring holes
to prevent dust or other conductive particles from entering the system.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
hazard of tilting
All rear anchoring brackets must be installed.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
- Use the installation kit 0H-9658 shipped with the bypass inductor cabinet. Fasten the angle to the right side of the rear anchoring bracket for the bypass inductor cabinet. Note the direction of the plate.
- Place the rear anchoring brackets for the bypass inductor cabinet, the I/O cabinet, and the power cabinets in the final installation area.
- Interconnect the rear anchoring brackets using the provided screws and bolts.
- Mark the hole locations.
- Drill anchoring holes according to the national and local requirements.
- Mount the rear anchoring brackets to the floor. Bolts are not supplied.
- Use a bubble-leveler to ensure that the rear anchoring brackets are level. Use the provided leveling shims if necessary.