Introduction
Overview of Configurations
Installation Kits Shipped inside the Frame
Installation Kit 0H-9658
Part | Used in | Number of Units |
---|---|---|
Angle for right side of the rear anchoring bracket 870- 66649 |
Mount the Rear Anchoring Brackets |
1 ![]() |
M8 x 25 hexagonal torx with washer |
3 ![]() |
|
Rear anchoring angle 0M-816922 |
1 ![]() |
|
Top baying cover 0M-95514 |
Position the Cabinets |
1 ![]() |
M6 x 16 torx screw with washer |
13 ![]() |
|
Front anchoring angle 0M-816915 |
Final Installation Steps |
1 ![]() |
M8 x 20 hexagonal torx with washer |
6 ![]() |