990-91735A-001

View the Communication Status and Start/Stop the Communication with the UPSs and External Disconnect Devices

  1. On the main menu screen, tap Communication. The color of the lines connecting the remote centralized display and the UPSs or the external disconnect devices in the diagram indicates the communication status.
    • Gray: UPS/external disconnect devices not present

    • Green: UPS/external disconnect devices present and communication is normal

    • Red: UPS/external disconnect devices present and communication is abnormal

  2. Tap Connect or Disconnect to start or stop the communication with each UPS or the external disconnect devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?