990-91735A-001

Configure the External Disconnect Devices

  1. On the main menu screen, tap Configuration > External breakers.
    1. Tap the buttons to configure which disconnect devices are Present or Not Present.
    2. Tap the button to configure the disconnect devices as Normally closed or Normally open.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?