Overview of User Interface
Overview of the Home Screen
-
Home button - tap this button on any screen to return to the home screen.
-
Main menu button - tap this button on any screen to access the menus.
-
Mimic diagram button - tap on the gray UPS to see the mimic diagram on UPS level.
-
Alarm status symbol - tap this button on any screen to access the active alarms log.
Main Menu
Menu Tree
-
Configuration*
-
System
-
Display
-
-
Logs
-
Communication
-
Control
-
External breakers
-
About
-
Logout
Some menus contain more submenus than described in this manual. These submenus are grayed out and are only for use by Schneider Electric to avoid unwanted load impacts. Other menu items can also be grayed out/not shown on the display if they are not relevant or not released yet for this particular UPS system.
Mimic Diagram
The home screen shows the mimic diagrams for parallel systems. Tap on each UPS to see the mimic diagram on UPS level.
The mimic diagram will adapt to your system configuration – the mimic diagrams shown here are just examples.
The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.
Alarm Status Symbol
The alarm status symbol (gray in illustration) in the top right corner of the display changes depending on the alarm status of the UPS system.
Green: No alarms present in the UPS system. | |
Blue: Informational alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log. | |
Yellow: Warning alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log. | |
Red: Critical alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log. |