990-91735A-001

Mount the Remote Centralized Display to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the remote centralized display to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate hardware (not supplied) to mount the remote centralized display to the wall.
Failure to follow these instructions can result in injury or equipment damage.
  1. Measure and mark the four mounting hole locations on the wall.
  2. Drill holes in each of the four marked locations.
  3. Open the front door of the remote centralized display.
  4. Line up the remote centralized display with the four holes on the wall and mount the remote centralized display to the wall with M8 screws and rawlplugs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?