Connect the Power and Signal Cables in a Modbus TCP Configuration
![]() |
---|
hazard of electric shock, explosion, or arc flash
Perform a total power off of the UPS system before connecting
the cables to the remote centralized display.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Risk of equipment damage
All Class 2/SELV signal cables
shall be double insulated cable and minimum rated for 30 VDC. All non-Class 2/non-SELV signal cables shall be double
insulated cable and minimum rated for 600 VAC.
Failure to follow these instructions can result in injury or equipment damage.
|
- Connect the large precabled connector to the digital input module TM3DI8 attached to the PLC with Ethernet ports.
- Connect the small precabled connector to the power port CN3 on the PLC with the Ethernet ports.
- Connect the provided signal cable 0W8130B between the display port ETH1 and the ConneXium switch port 1.
- Connect the provided signal cable 0W8130B between the Ethernet port CN1 on the PLC and the ConneXium switch port 2.
- Route the RJ45 cables from each UPSs through the bottom of the remote centralized display and connect to the ConneXium switch port 3-8. UPS 1 to port 3, UPS 2 to port 4, UPS 3 to port 5, UPS 4 to port 6, UPS 5 to port 7, UPS 6 to port 8.
- Route the signal cables from the external disconnect devices in the switchgear (MBB, SIB, 0DB1, 0DB2, 0DB3, 0DB4, 0DB5, LBB) through the bottom of the remote centralized display and connect to the communication terminal block.
- Remove the transparent protection cover in front of the
power terminals. Route the power cables through the bottom of the
remote centralized display and connect to the power terminal block:
- Connect the PE cables to the power terminals.
- Connect the power cables to the power terminals AC INPUT 1 (L1, L2, L3) and AC INPUT 2 (L1, L2, L3).
- Reinstall the transparent protection cover in front of the power terminals.