EIO0000003790.05

Installing Using Spring Clips

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
Failure to follow these instructions will result in death or serious injury.
CAUTION
SPRING LOADED MECHANISM
Do not release the spring clip mechanism near your face.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
EQUIPMENT DAMAGE
  • Always use the installation gasket.
  • Keep this product stabilized in the panel-cut while you are installing or removing the fasteners.
Failure to follow these instructions can result in equipment damage.
  1. Place this product on a clean and level surface with the screen facing down.
  2. Check that this product's gasket is seated securely into the bezel's groove, which runs around the perimeter of the display frame.
    NOTE: Always use the installation gasket, since it absorbs vibration in addition to repelling water. For the procedure on replacing the installation gasket, refer to Replacing the Installation Gasket.
  3. Based on this product's Panel Cut Dimensions, open a mount hole on the panel and attach this product to the panel from the front side.
    NOTE: This product has a hook at the top to prevent it from falling. Insert the bottom part of the product into the panel opening, and then insert the top part while pushing the hook down.

    1 Hook

  4. Press the spring clip hooks into the insertion slots on this product. Adjust the spring clips for the panel thickness by turning it over:
    • Position 1

      1.5 mm (0.059 in) ≤ panel thickness ≤ 4 mm (0.157 in).

    • Position 2

      4 mm (0.157 in) ≤ panel thickness ≤ 6 mm (0.236 in).

    Side of the spring clip

    1 Hook for position 1

    2 Hook for position 2

    3 Insertion slots

  5. Lock the spring clips by simultaneously pressing the top and bottom of the clip.

    1 Installation panel

    2 Spring clip

  6. To remove the spring clips, unlock the clips by pressing on the back of the clip until you hear a click.

CAUTION
RISK OF INJURY
Do not drop this product when you remove it from the panel.
  • Hold this product in place after removing the spring clips.
  • Use both hands.
  • While pushing on the hook, be careful not to hurt your fingers.
Failure to follow these instructions can result in injury or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.