EIO0000003790.05

System Design

Product Overview

This product is an industrial display equipped with a dedicated HTML5-compatible browser. As a Web client, the product can access Web servers on the same Intranet and display the server content in the dedicated browser.

  • Can connect to HTML5 servers (such as HMI, IPC, PLC, and other external devices with Web server functionality*1) that support Java Script. You can connect to up to 10 web server devices.

  • The dedicated browsers support CSS3 and XML.

  • You cannot use this product on the Internet.

  • HMI applications do not run on this product.

After turning on this product, you need to set up its display and Web browser settings. For information about settings, refer to Display/Browser Settings.

*1 For supported models, please contact customer support.
www.se.com

System Structure

This section describes the system configuration with this product and peripheral equipment.

*1 Refer to Accessories.

*2 A USB storage device, USB keyboard, USB mouse, and USB hub can be used. Multiple USB devices of the same type cannot be connected.

*3 Only for HMISTW6200, an Ethernet hub is required to connect to the Intranet.

*4 For supported models, please contact customer support.
www.se.com

NOTE:
  • The number of Ethernet interfaces varies depending on the model. Refer to Parts Identification.

  • Connect USB devices before turning on the product.

  • When a USB keyboard is connected, the software keyboard is not displayed.

  • Use a FAT32 formatted USB storage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.