EIO0000003790.05

Update the System

Updates the product system with the system file saved on USB storage.
  1. Prepare a USB storage device (formatted to FAT32).
  2. Download the system update file for this product from our website.
    https://www.se.com/ww/en/faqs/FA403854/
  3. Unzip the downloaded file and save all files to the root folder of the USB storage device.
  4. Connect the USB storage device to the product and turn on the product.
  5. Display the Configuration Menu. Refer to How to Display Configuration Menu.
  6. Touch System, then under Update System touch the Update button. In the message that displays, touch OK.
  7. The update process is started. Please wait a moment until the process is complete. When prompted to restart, touch OK.
  8. After restarting the product, verify that the system has been updated. Display the browser title bar and touch the Menu icon > Information icon, in that order.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.