Operation of Web Browser
No. |
Description |
---|---|
1 |
Displays the title of the Web server page or the URL when the page does not have a title. |
2 |
Each time you touch this icon, the displayed Web server changes. NOTE: The server switching icon is available for products with system
version V1.1.0 or later.
|
3 |
Moves to the previous page. |
4 |
Moves to the next page. |
5 |
Icon that displays while loading the Web server screen. Touch this icon to interrupt the load operation. |
6 |
Reloads the Web server screen. Touch this icon and when the load operation starts, the icon changes to the No.5 icon. |
7 |
Displays the Web server screen set in Server > Start Page. |
8 |
Touch this icon to display the A sub menu. |
9 |
Touch this icon to display the B sub menu, where you can select the Web server to display. |
10 |
Touch this icon to display the C sub menu, where you can adjust the zoom level from 25 to 500%. The default setting is [100%]. C-1 is the reset button. |
11 |
Displays the system version, network, current usage and license information. |
12 |
Displays the Configuration Menu. |
13 |
Displays the selected Web server screen. |
14 |
Touch the screen to display these scroll buttons. You can hide these arrows with Boot > Hidden Scroll Arrow. |