EIO0000003790.05

Parts Identification (HMISTW6400)

Front

Top

Bottom

Rear

A: Status LED

B: Battery slot*1

C: Hook

D: Ethernet interface (ETH2)*2

E: Ethernet interface (ETH1)*2

F: Power plug connector

G: USB (Type A) interface

H: USB (micro-B) interface*3

*1 Products do not have a battery.

*2 ETH1 and ETH2 have the same IP address and MAC address.

*3 The USB (micro-B) interface is unavailable.

NOTE: This product does not have serial interfaces (COM1 and COM2).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?