7EN02-0418-02

Configuring network parameters

  1. Navigate to Menu > Settings > Network.

    The NETWORK screen displays.

  2. Modify the parameters value as per the following table:
    NOTE: Use the contextual menu buttons to modify the parameters value.
    Parameter Allowed Values Default Value Description
    App
    • Power C.

    • Control C

    • Photovolt

    Power C

    • Select Power C for industrial or marine applications that contain power loads and power electronics such as speed drives, inverters, or rectifiers.

    • Select Control C for auxiliary control circuits used to drive power systems which contain sensitive loads such as PLCs, IOs, or sensors.

    • Select Photovolt for large photovoltaic power generation systems.

    NOTE: If you select Photovolt,
    • Locating value is set to OFF

    • V.Adapt value is set to HV1700C

    • Frequency value is set to DC

    Filtering
    • 4s

    • 40s

    • 400s

    40s

    Select the filtering time depending on the application.
    NOTE: This value selection is restricted depending on the App value selection.
    Locating
    • OFF

    • Prev.Al.

    • Alarm

    • IFL

    Alarm

    • Select Alarm if boost mode is required in case of active insulation alarm and Insulation resistance is less than 2 KΩ (if using XD312 as fault locator).

    • Select Prev.Al if boost mode is required in case of active preventive insulation alarm and Insulation resistance is less than 50 KΩ (if using XD312H as fault locator).

    • Select IFL if boost mode is required in case of active preventive insulation alarm and Insulation resistance is less than 2 KΩ (if using IFL12, IFL12MC, IFL12LMC, IFL12MCT, and IFL12LMCT as fault locator).

    NOTE:
    • If you select Prev.Al., you need to select the preventive alarm threshold.

    • This value selection is restricted depending on the App value selection.

    V.Adapt
    • None

    • VA2

    • PHT1000

    • HV1700C

    None

    Select the adaptor if the network voltage is greater than the rated network voltage of the device.
    NOTE: This value selection is restricted depending on the App value selection.
    Frequency
    • 50 Hz

    • DC

    • 400 Hz

    • 60 Hz

    50 Hz

    Select the rated frequency of the monitored power system.
    NOTE: This value selection is restricted depending on the App value selection.
    HRG
    • OFF

    • 0.1....2 MΩ

    OFF

    • Select OFF when no grounding resistance is connected.

    • Select the value of the neutral grounding resistance, which is connected to the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.