JYT3013100

Before Energizing for the First Time

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS,  CSA Z462, or local equivalent.
  • Equipment must be installed, operated, and serviced only by qualified electrical personnel. Only qualified personnel familiar with medium voltage equipment are to perform work described in this set of instructions. Workers must understand the hazards involved in working with, or near medium voltage circuits.
  • Perform all checks with the entire switchgear de-energized.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Check the switchgear to make sure the shipping brackets of the EvoPacT circuit breaker have been removed.
  • Check that the left and right lifting brackets on the sides of the circuit breaker have been removed (if the circuit breaker did not come installed in the switchgear).
  • Never insert a circuit breaker into a circuit breaker compartment that is not complete and functional.
  • Do not use a circuit breaker that shows signs of damage. Inspect insulator barriers, supports, and covers for cracks prior to use.
  • Use only a circuit breaker that is unmodified, complete, properly rated, and functional.
  • Handle this equipment carefully and install, operate, and maintain it correctly in order for it to function properly. Neglecting fundamental installation and maintenance requirements may lead to personal injury, as well as damage to electrical equipment or other property.
  • Beware of potential hazards. Carefully inspect the work area and remove any tools or objects that may have been left on or inside the equipment.
  • Store, install, and operate the electrical equipment only in the environment for which it was designed.
  • Check that nameplate data is compatible with that of the electrical installation.
  • Check the customer order drawings and the nameplates, compare the secondary disconnect labels on the circuit breaker and the circuit breaker compartment, and check the mimic diagram (if equipped) on the front of the section to verify the circuit breaker is installed into the proper circuit breaker compartment.
  • Check the correct operation of the MX, XF, and MN auxiliary releases.
Failure to follow these instructions will result in death or serious injury.

A general check of the circuit breaker takes only a few minutes and reduces the risk of mistakes due to errors or negligence. Examine the entire circuit breaker for damage, dirt, moisture, and signs of previous moisture presence. Use a clean, dry, lint-free cloth to remove any dirt or particulates that may have collected on the insulating parts. Prior to operating the circuit breaker, contact the local Schneider Electric Service representative if there are any signs of damage or moisture.

Before initially installing the circuit breaker into its compartment, first energization following installation, or re-energization following an extended out of service period for the circuit breaker, perform the following procedures:

After performing all procedures be sure to:

  1. Remove all tools and miscellaneous items left on or inside the circuit breaker.

  2. Replace all devices and circuit breaker covers.

The installer of the equipment must deliver a commissioning report before electrical installation is energized for the first time.

Initialization of the Maintenance Information

For record-keeping and follow-ups of the equipment, upload all installation, commissioning, usage, and maintenance information to the Schneider Electric Safe Repository. Record the number of circuit breaker operations (as displayed on the operation counter) and the date upon initial operation of the circuit breaker.

Switchgear Inspection

Check that the switchgear and circuit breakers are in good serviceable condition. They must be clean and free of any installation scraps or items (tools, electrical wires, broken parts or shreds, metal objects, etc.).

For reference, the secondary disconnect plug for circuit breaker power and control in EvoPacT circuit breaker cradles and SureSeT switchgear is located at the front, top, center area of the circuit breaker. The circuit breaker has a molded plug containing 33 contacts as standard, but it may be equipped instead with a “Contact Plus” plug that offers more circuit breaker auxiliary contacts, provides indication of the status of the plug, offers a provision for the close blocking magnet, and has an increased number of racking endurance operations (see the table Secondary Disconnect Labels).

The type of plug on the circuit breaker must be coordinated with and match the type of receptacle in the circuit breaker compartment. This coordination is indicated by the symbols on the labels on the circuit breaker compartment bracket and on the circuit breaker plug cover (see the table Secondary Disconnect Labels and the figure Coordinating Circuit Breaker Compartment and Circuit Breaker Secondary Disconnect Labels).

The secondary disconnect plug for circuit breaker power and control engages with two tapered guide pins on the compartment of the receptacle mounting assembly. Physically, the test and disconnected positions on the racking mechanism are the same. When the circuit breaker is fully racked out, it moves to the test/disconnected position and the secondary disconnect plug for power and control is automatically disconnected. When the receptacle in the compartment is manually pulled forward to connect with the circuit breaker in the test/disconnected position, the circuit breaker is placed into test mode.

Control power can be manually connected to the circuit breaker in the test/disconnected position by pulling the handle attached to the secondary disconnect receptacle in the compartment forward to mate with the circuit breaker plug (refer to the section Secondary Disconnect Plug for Circuit Breaker Power and
Control — Operation and Testing the Circuit Breaker in the Test/Disconnected Position
for further information). Check the customer order drawings and the nameplates, and compare the secondary disconnect labels on the circuit breaker and the circuit breaker compartment (see the figure Coordinating Circuit Breaker Compartment and Circuit Breaker Secondary Disconnect Labels) to verify the circuit breaker is installed into the proper circuit breaker compartment.

Secondary Disconnect Labels

Secondary Disconnect Label

Secondary Disconnect Plug for Circuit Breaker Power and Control

Breaker Features

Maximum Number of Racking Operations

Number of Auxiliary Contacts

None (standard)

Standard

Digital Ready

500

5NO, 4 NC

Contact Plus

Digital Ready

1000

10NO, 9NC

Standard

Digital Monitoring and/or Digital Control

500

5NO, 4 NC

Contact Plus

Digital Monitoring and/or Digital Control

1000

10NO, 9NC

Coordinating Circuit Breaker Compartment and Circuit Breaker Secondary Disconnect Labels

Label on circuit breaker compartment identifying type of secondary disconnect receptacle for circuit breaker power and control

Label on circuit breaker identifying type of secondary disconnect plug for circuit breaker power and control

NOTE: Before racking in the circuit breaker, verify the label (A) on the switchgear circuit breaker compartment and the label (B) on the circuit breaker to be used in the compartment correspond with each other.

Compliance with the Installation Electrical Diagram(s)

WARNING
NON-COMPLIANT VOLTAGE
Apply the assigned voltage for the control auxiliaries and check it directly on the auxiliary terminals.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Check that the circuit breakers match the installation diagram/customer order drawings for:

  • breaking capacities indicated on the nameplates

  • presence of optional functions (electric control of charging mechanism, racking mechanism motor control, auxiliaries, meters, blocking magnet and indicators, etc.) and compliance with their electrical settings

  • identification of the applicable circuit on the front of the circuit breakers and/or SureSeT switchgear

  • verification that the secondary disconnect plug for circuit breaker power and control and the compartment receptacle correspond or match by comparing the secondary disconnect labels on the circuit breaker and the circuit breaker compartment (see the figure Coordinating Circuit Breaker Compartment and Circuit Breaker Secondary Disconnect Labels)

Operation Checks

Refer to the switchgear documentation and follow the commissioning rules that pertain to the switchgear. The initial state of the EvoPacT circuit breaker is the open (O OPEN) position with all springs discharged and the racking mechanism in the test/disconnected position. Verify this state by checking the circuit breaker and racking mechanism indicators. If it is not in this position, manually press the open (O OPEN) push button, the close (I CLOSE) push button, and then the open (O OPEN) push button again or use the racking/charing handle with the racking mechanism to move into the test/disconnected position (refer to Using the EvoPacT Circuit Breaker, for further information on performing the procedures in this section).

NOTE: The circuit breaker is normally shipped in the closed (I CLOSED) position.

Initial State of the EvoPacT Circuit Breaker


Check the mechanical operation of the circuit breakers several times in every control mode (local mechanical and electrical controls and remote control) and for every possible operation for proper functionality:

  • close the circuit breaker

  • open the circuit breaker

  • close the circuit breaker and perform an operation sequence OPEN - CLOSE - OPEN

  • rack-in and rack-out the circuit breaker (according to the configuration of the switchgear)

  • in case of racking mechanism motor control:

    • energize the racking motor from the low voltage compartment

    • rack-in and rack-out the circuit breaker (according to the configuration of the switchgear)

    • de-energize the racking motor from the low voltage compartment

  • check the operation of the locking and interlocking.

Remove all tools and miscellaneous items left on or inside the circuit breaker. Replace all devices and circuit breaker covers and place the EvoPacT circuit breaker back into its initial state while waiting for the switchgear to be energized.

For reference, the circuit breaker and the SureSeT circuit breaker compartments are equipped with an interlock system designed to:

  • not allow the circuit breaker to be inserted into the compartment if the circuit breaker is not in the fully racked out position. The circuit breaker is blocked by a plate in the compartment and the locking tabs are blocked from retracting, preventing latching into the compartment plates.

  • not allow the circuit breaker to be pushed into the compartment when the circuit breaker is closed (I CLOSED). The automatic discharge pin of the circuit breaker is operated by a plate in the circuit breaker compartment.

  • not allow the circuit breaker to be closed (I CLOSED) while it is moved between the test/disconnected and connected position (due to an interlock integrated on circuit breaker)

  • not allow the circuit breaker to be moved from the connected position when it is closed (I CLOSED) (due to an interlock integrated on circuit breaker)

  • discharge both the closing and trip springs when the circuit breaker is being removed (withdrawn) from the circuit breaker compartment. The automatic discharge pin of the circuit breaker is operated by a plate in the circuit breaker compartment.

Initial E-gap Measurement

The erosion gap or E-gap should be measured, outside the switchgear circuit breaker compartment, before the initial installation of the circuit breaker. Refer to Maintaining the Performance of the EvoPacT Circuit Breaker and Maintenance E-gap Measurement for more details on measuring the E-gap during the life of the circuit breaker.

The E-gap is the space between the bottom of the pivot block and the top surface of the hexagonal end of the bias spring sleeve. The pivot block and bias spring sleeve are located below each of the vacuum interrupters at the bottom of the pole assembly (refer to E-gap). Follow steps 1–7 to measure and record the initial E-gap.

  1. Manually charge the circuit breaker and push the close (I CLOSE) push button.

  2. Use pin gauges, feeler gauges, or drill bits to measure the space between the pivot block and the hexagonal block.

    E-gap Settings

    Short Circuit Current Rating

    Initial E-gap

    <40 kA

    0.118 ± 0.016 in.
    (3.0 ± 0.4 mm)

  3. The E-gap is factory set and should not be adjusted, only measured.

  4. Record the initial E-gap measurement in the maintenance log on the Schneider Electric Safe Repository.

    NOTE: It is important to keep this measurement to compute the contact erosion during the life of the circuit breaker.

  5. Push the open (O OPEN) push button.

  6. Remove all tools and miscellaneous items left on or inside the circuit breaker.

  7. Replace all devices and circuit breaker covers.

E-gap

A

Nylock nut

B

Hexagonal end of bias spring sleeve

C

E-gap (distance between the bottom of “D” and the top of “B”)

D

Pivot block

Initial Dielectric Withstand Test

DANGER
hazard of electric shock, explosion, or arc flash
When performing the dielectric withstand test:
  • Do not exceed the voltages shown in One-Minute High-Potential Dielectric Withstand Test Levels.
  • Keep all persons at least 6 ft. (2 m) away from the circuit breaker being tested.
  • Discharge to ground the primary high voltage contacts (i.e., runbacks and clusters) and the vacuum interrupter mid-band ring before handling the circuit breaker. These areas can retain a static charge after a dielectric withstand test.
Failure to follow these instructions will result in death or serious injury.

One-Minute Dielectric Withstand Test Levels

Equipment Rating

Field Test Voltage

AC

DC

5 kV

14 kV

20 kV

15 kV

27 kV

38 kV

NOTE: AC voltages are 60 Hz, rms symmetrical.

Follow the steps below to perform the dielectric withstand tests. If the equipment does not sustain the specified voltage for one minute without flashover, inspect the insulators for leakage paths. If necessary, clean the surface of each insulator and repeat the test.

NOTE: Consistent, unacceptable results may indicate a loss of vacuum. Contact the local Schneider Electric representative.
  1. Check the circuit breaker indicators to verify that the circuit breaker is in the open (O OPEN) position with all springs discharged (refer to The Circuit Breaker Indicators). If it is not in this position, press the open (O OPEN) push button, the close (I CLOSE) push button, and then the open (O OPEN) push button again (refer to Typical EvoPacT Circuit Breaker Features.

  2. Ensure that all persons are at least 6 ft. (2 m) away from the circuit breaker being tested.

  3. Perform a line-to-load (across the open vacuum interrupter contacts) dielectric withstand test on each pole:

    1. Gradually increase the voltage to the levels indicated in One-Minute Dielectric Withstand Test Levels.

    2. Verify that the circuit breaker sustains the specified voltage without flashover for one minute.

    3. After the test is complete, discharge to ground the primary high voltage contacts (i.e., runbacks and clusters) and the vacuum interrupter mid-band ring before handling the circuit breaker.

    4. Repeat the steps on each vacuum interrupter assembly.

  4. After the circuit breaker has been fully discharged to ground, close the circuit breaker by pressing the close (I CLOSE) push button (refer to Typical EvoPacT Circuit Breaker Features).

  5. Perform a phase-to-phase dielectric withstand test on each pole:

    1. Gradually increase the voltage to the levels indicated in One-Minute Dielectric Withstand Test Levels.

    2. Verify that the circuit breaker sustains the specified voltage without flashover for one minute.

    3. After the test is complete, discharge to ground the primary high voltage contacts (i.e., runbacks and clusters) and the vacuum interrupter mid-band ring before handling the circuit breaker.

    4. Repeat the steps on each vacuum interrupter assembly.

  6. Perform a phase-to-ground dielectric withstand test on each pole:

    1. Gradually increase the voltage to the levels indicated in One-Minute Dielectric Withstand Test Levels.

    2. Verify that the circuit breaker sustains the specified voltage without flashover for one minute.

    3. After the test is complete, discharge to ground the primary high voltage contacts (i.e., runbacks and clusters) and the vacuum interrupter mid-band ring before handling the circuit breaker.

    4. Repeat the steps on each vacuum interrupter assembly.

  7. After the circuit breaker has been fully discharged to ground, press the open (O OPEN) push button, the close (I CLOSE) push button, and then the open (O OPEN) push button again (refer to Typical EvoPacT Circuit Breaker Features to return the circuit breaker to the initial state of open (O OPEN) with all springs discharged (refer to the section The Circuit Breaker Indicators).

  8. Remove all tools and miscellaneous items left on or inside the circuit breaker.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.