JYT3013100

Using the EvoPacT Circuit Breaker

Circuit Breaker Overview

Circuit Breaker Mechanism Area


A

Wiring module

B

MOC (optional)

C

Auxiliary contact switch

D

Charging mechanism with M1 electrical motor

E

Electromagnet interlock assembly for the circuit breaker racking mechanism (optional)

F

ARF200 operating mechanism

G

Operation mechanism charging handle port

H

Mechanical operation counter

I

Spring charged status indicator

J

Open-Close main contact position indicators

K

S2 spring charge indication contact

L

MX2 or MN opening release coil (optional)

M

MX1 opening release coil

N

Closing springs

O

XF closing release coil

P

Automatic discharge pin

Q

Blocking magnet for circuit breaker closing

R

TOC pin

S

Secondary disconnect plug for circuit breaker power and control

NOTE: Front cover, auxiliary contact switch cover plate, anti-pump relay cover plate, and secondary disconnect plug cover removed for clarity.

Vacuum Bottle Interrupters

The Schneider Electric brand vacuum interrupters (VI’s), which are mounted vertically on the back side of the circuit breaker frame, perform the circuit breaker interruption (see Typical EvoPacT Circuit Breaker Features). There is one VI for each phase, assembled in an insulation housing and connected to the circuit breaker contact pads. The VI’s consist of a pair of contacts, one movable and one fixed. The VI’s require only a short contact gap for circuit interruption.

Primary High Voltage Contacts (Runbacks and Clusters)

The primary connection of the circuit breaker to the associated switchgear is through the six primary high voltage contacts consisting of the runbacks and clusters mounted horizontally at the rear of the circuit breaker (see Typical EvoPacT Circuit Breaker Features).

ARF200 Operating Mechanism

The EvoPacT circuit breaker uses a stored energy type operating mechanism that is independent of operator input, providing correct opening and closing speeds. It uses charged springs to perform circuit breaker opening and closing functions. It is mounted at the front of the circuit breaker for easy access during inspection and maintenance (see the figure Circuit Breaker Mechanism Area).

Principle of Operation

The closing springs are charged, either manually or using the M1 electrical motor. The energy stored in the closing springs is released using the XF coil or closing push button. As the mechanism closes the circuit breaker, the opening spring is charged using the energy of the closing springs and the circuit breaker is latched closed (I CLOSED). To open the circuit breaker, the opening spring energy must be released; this is accomplished using the opening push button, or MX or MN opening releases.

Mechanical Operation Counter

The mechanical operation counter shows the number of opening/closing cycles performed by the circuit breaker. It is located in the middle of the circuit breaker ARF200 operating mechanism and can be seen through a window in the front cover (see Typical EvoPacT Circuit Breaker Features and Circuit Breaker Mechanism Area). When the customer receives the circuit breaker, the number of cycles will not be zero due to functional tests and controls performed in the factory. Typically, the counter will show approximately 100 cycles.

Closing Springs

The closing springs close the circuit breaker when the close (I CLOSE) push button is pressed or when the XF closing release coil is energized (refer to Closing the Circuit Breaker). The closing spring assembly is located to the right of the ARF200 operating mechanism (see Circuit Breaker Mechanism Area). These springs are charged (compressed) either manually with the manual racking/charging handle or electrically by the spring charging motor (refer to Charging the Operating Mechanism).

When control power is applied to the circuit breaker, the spring charging M1 electrical motor is energized. The charging motor turns the gear box gears, which drive the ratchet assembly up and down. The ratchet assembly rotates the drive shaft compressing the closing springs. As the spring loads pass top dead center, the drive shaft rotates a few degrees until the closing latch roller engages the closing latch. The drive shaft can rotate no further; the closing springs are held in this charged position until a closing operation is initiated by the close (I CLOSE) push button or closing release coil.

Opening Spring

The opening spring opens the circuit breaker when the open (O OPEN) push button is pressed or the opening coil is energized. The opening spring with an operation damper is located on the left side of the ARF200 operating mechanism behind the auxiliary switch. This spring is compressed whenever the circuit breaker is in the closed position.

Understanding the Circuit Breaker Controls and Indicators

The Circuit Breaker Indicators

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, or CSA Z462 or local equivalent.
  • Installation, repair, and maintenance work on the circuit breaker must only be carried out by qualified personnel.
Failure to follow these instructions will result in death or serious injury.

The ARF200 operating mechanism has indicators visible through two windows on the front cover of the circuit breaker (see Typical EvoPacT Circuit Breaker Features and Circuit Breaker Mechanism Area). The open (O OPEN)-closed (I CLOSED) indicators show whether the vacuum bottle interrupter main contacts are open or closed. The charged-discharged indicator shows whether the circuit breaker closing spring is charged or discharged. Refer to the table below for more details.

     

Circuit Breaker Indicators

Electrical State State Description Command Available
Main Contacts Position Indicator Spring Charged Status And “Ready to Close” Indicator
Circuit breaker is open (O OPEN) and operating mechanism is discharged. Charging the operating mechanism (refer to Charging the Operating Mechanism)
Circuit breaker is open (O OPEN) with operating mechanism charged. Closing of the circuit breaker (refer to Closing the Circuit Breaker)
Circuit breaker is closed
(I CLOSED) and operating mechanism is discharged.
Circuit breaker is closed
(I CLOSED) and operating mechanism is charged.

Local Control

Circuit breaker operations can be mechanically controlled on the circuit breaker or electrically controlled by using the control devices on the switchgear front panels.

Mechanical control

A mechanical operation on the circuit breaker allows the user to:

  • store the energy required to open or close the circuit breaker; the racking/charging handle enables the manual charging of this mechanism.

  • control the state of the circuit breaker (open (O OPEN) or closed (I CLOSED)) with the push buttons located on the front face of the circuit breaker.


A mechanical operation on the racking mechansim allows the user to:

  • perform circuit breaker racking in/racking out

  • operate the red racking/emergency trip push button of the racking mechansim.

Electrical Control

In order to use the electrical control functions, either local or remote, the electrical auxiliary controls must be installed.

The table below shows the possible configurations for electrical control of the circuit breaker.

Charging Devices Closing Release Opening Releases Racking Mechanism Motorization Circuit Breaker Electromagnetic Close Interlock Electromagnetic Racking Interlock

M1

S2

XF

MX1

MX2

MN

     
   

Optional

Optional

Optional

 

Optional

Optional

Optional

 

Optional

Optional

Optional

Refer to the switchgear documentation to find out where the circuit breaker control buttons are located.

Remote Electrical Control

Remote electrical control allows the user to perform circuit breaker operations at a distance. To use the electrical control functions, the electrical auxiliary controls must be installed (see the Electrical Control table in the Local Control section).

Refer to the switchgear documentation to find out the available communication functions.

Charging the Operating Mechanism

Manual Charging

WARNING
excessive torque applied to equipment
Do not charge the ARF200 operating mechanism using a power drill.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Perform the following steps to manually charge the operation mechanism:

  1. Move the circuit breaker into a “ready to close” position by checking that the circuit breaker is in the test/disconnected position.

    NOTE: The circuit breaker can be charged if it is in either the open (O OPEN) or closed (I CLOSED) state.
  2. Insert the racking/charging handle into the opening for tensioning the operation mechanism.

  3. Rotate the racking/charging handle clockwise to charge the operation mechanism as illustrated. (The effective rotation angle is 180°.) Charging should take approximately 12 full rotations of the handle. As soon as the mechanism is fully charged, the operation mechanism is uncoupled and the status indicator signals “Charged/OK”. Rotating the handle further will not damage the mechanism.

  4. Remove the racking/charging handle.

  5. The circuit breaker is ready for closing.

Mechanism status indicator signaling it is “charged” and that the circuit breaker can be closed (I CLOSED).


Automatic Charging by the M1 Electrical Motor

The ARF200 operating mechanism of motorized circuit breakers is charged automatically as soon as the auxiliary voltage is applied by the closing of the S2 spring charge indication limit switch (refer to The Circuit Breaker Indicators, and S2 “Spring Charge Indication” Contact for more information). The spring charging assembly is located on the left side of the ARF200 operating mechanism (see the figure Circuit Breaker Mechanism Area). If the spring charge motor is supplied with an adequate power supply, the mechanism is automatically charged each time the circuit breaker completes a close operation (refer to Typical Circuit Breaker Electrical Schematic for further details).

When energized by the closing of the S2 limit switch, the M1 spring charging motor drives a series of connected gears which, in turn, operate the ratchet assembly to rotate the drive shaft. As the drive shaft rotates, the closing springs compress to the charged position. When the closing springs are fully charged, the S2 limit switch contacts reopen, de-energizing the M1 spring charging motor.

S2 “Spring Charge Indication” Contact

The circuit breaker closing spring charged status indication is provided both mechanically by a mechanical indicator through a window on the front cover of the circuit breaker (see The Circuit Breaker Indicators) and electrically by a changeover limit switch (S2). The S2 limit switch assembly is located on the lower right side of the ARF200 operating mechanism (see the figure Circuit Breaker Mechanism Area). The limit switch contact is internally wired to the spring charging M1 electrical motor and energizes the motor as soon as the spring is discharged in order to provide quick recharging for reclosing operations (refer to Typical Circuit Breaker Electrical Schematic for further details). The motor limit switch de-energizes the spring charging motor when the closing springs reach the fully charged position. One additional contact is also wired to the “ready to close” indication of the breaker (refer to “Ready to Close” Indication for further information).

S4 “Open Signal Indication” Contact

The presence of an active trip signal on the circuit breaker is provided by a changeover limit switch (S4) (refer to Typical Circuit Breaker Electrical Schematic for further details). It is located on the upper left side of the ARF200 operating mechanism behind the auxiliary switch. It is wired to the “ready to close” indication of the breaker (refer to “Ready to Close” Indication for further information).

“Ready to Close” Indication

DANGER
anti-pump loss
Do not wire the ready to close indication in series to the closing release XF.
Failure to follow these instructions will result in death or serious injury.

In order to execute a closing operation using the closing (I CLOSE) push button or the XF closing release coil, the following conditions must be satisfied:

  1. The circuit breaker contacts are in the open (O OPEN) position (electrical indication provided by the circuit breaker auxiliary switch, S11)

  2. The closing spring of the circuit breaker mechanism is charged (electrical indication provided by the spring charge limit switch, S2)

  3. No trip signal is applied to the circuit breaker ARF200 operating mechanism via the opening (O OPEN) push button, the red racking/emergency trip push button, or any of the opening releases (MX1, MX2, and MN) (electrical indication provided by trip half-moon limit switch, S4)

  4. The close signal that caused the previous circuit breaker closing operation has been reset.

  5. The circuit breaker is not in the transport position.

When these five conditions occur simultaneously, the circuit breaker is in a "ready to close" state.

The EvoPacT circuit breaker is provided with electrical indication of the “Ready To Close” conditions. Three internally wired switchcover contacts, each indicating one of the aforementioned conditions, are connected in series and wired to two pins of the secondary disconnect plug for circuit breaker power and control (refer to Typical Circuit Breaker Electrical Schematic) for further details.

Electrical continuity is only provided between the two secondary disconnect plug pins if all conditions required to execute a closing operation are met. This feature may be used to indicate to external devices that the breaker is ready to be successfully closed.

Do not wire the ready to close indication in series to the closing release XF. Doing so would defeat the mechanical anti-pumping function of the breaker mechanism (refer to Anti-Pump Function) for further information.

Closing the Circuit Breaker

Closing Conditions

NOTICE
inoperable equipment
Make sure the circuit breaker is in "ready to close" state before closing.
Failure to follow these instructions can result in equipment damage.

To close the circuit breaker, the circuit breaker must be in the "ready to close" state, established by simultaneously fulfilling the following conditions:

  • circuit breaker is open (O OPEN)

  • circuit breaker mechanism closing spring is charged as shown by the spring charged status/"ready to close" indicator

  • no opening order is activated by:

    • an opening release (MX1, MX2, or by optional MN)

    • an ongoing mechanical open operation (i.e. either the open (O OPEN) pushbutton or the red racking/emergency trip push button pushed in)


Manual Closing (local)

After the circuit breaker is in the “ready to close” state, to perform a manual closing of the circuit breaker primary contacts, push the closing (I CLOSE) push button.

The circuit breaker indicators move to the closed (I CLOSED) state and the spring charged status/“ready to close” indicator goes to the discharged state shown below.

If the M1 electrical motor for electrical charging is energized, the closing mechanism is automatically charged (< 7 seconds at rated control voltage) and the circuit breaker indicators will move to the state shown below.

Closing by Electrical Control

By adding the XF closing release, the circuit breaker can be closed by electrical control.


Local


XF Closing Release Coil

Refer to the switchgear documentation or customer order drawings to find out where the circuit breaker closing push button or breaker control switch is located.


Remote

Connect the remote control device to the XF closing release.

Refer to the switchgear factory drawings for the remote closing connection provisions.

Opening the Circuit Breaker

Opening Conditions

The opening order has priority over any other command.


Manual Opening (local)

To perform a manual opening (O OPEN) of the circuit breaker primary contacts, push the opening push button located directly on the circuit breaker operating interface.

In emergency situations, the red racking/emergency trip push button on the racking mechanism can also be used to trip open the circuit breaker (see the figures in the Red Racking/Emergency Trip Push Button section).

With the circuit breaker closing springs not charged prior to the open (O OPEN) operation, the circuit breaker contact position indicator moves to the open (O OPEN) state and the spring charged status/"ready to close" indicator remains in the discharged state as they are shown below.

With the circuit breaker closing springs charged prior to the open (O OPEN) operation, whether by a manual charging operation or an energized M1 electrical motor, the circuit breaker contact position indicator moves to the open (O OPEN) state and the spring charged status/"ready to close" indicator remains in the charged state as they are shown below.

Opening by Electrical Control

The circuit breaker can be electrically opened using the following auxiliaries (refer to Circuit Breaker Open and Close Coils and Typical Circuit Breaker Electrical Schematic for further details):

  • MX1: opening release

  • MX2: secondary opening release

  • MN: under-voltage opening release

MX1 Opening Release Coil

MX2, MN Opening Release Coils

 

Local

Refer to the switchgear documentation or customer order drawings to find where the circuit breaker opening push button or breaker control switch is located.


Remote

Connect the remote control devices to the opening releases of the circuit breaker. Refer to the switchgear factory drawings for the remote opening connection provisions.

Discharging the Mechanism

To discharge the mechanism:

  • Turn off the auxiliary control power supply or disconnect the secondary disconnect plug for circuit breaker power and control (the circuit breaker must be in the test/disconnected position to do so) to disable the electrical automatic spring charge.

  • Push alternately the opening (O OPEN) and closing (I CLOSE) push buttons until the state indicators of the circuit breaker are open (O OPEN) OFF / "Discharged" (state shown below).

Circuit Breaker Equipped With an MN Under-Voltage Opening Release

The MN under-voltage opening release coil provides a means for opening the circuit breaker upon auxiliary control power loss (refer to Circuit Breaker Open and Close Coils, for further information on the MN and other release coils). It is located in the typical coil mounting location on the top center of the ARF200 operating mechanism (see Circuit Breaker Mechanism Area).

When the MN under-voltage opening release is not energized, it provides a latched opening signal to the circuit breaker. The circuit breaker will immediately open and stay in the open position until:

  1. the MN under-voltage release is energized and

  2. a close command is applied to the breaker

For commissioning and testing of a circuit breaker equipped with a MN under-voltage opening release, ensure control power is applied across the release terminals in order to allow for circuit breaker closing operations.

Refer to Typical Circuit Breaker Electrical Schematic and the switchgear factory drawings to identify the MN under-voltage opening release connection points to its power supply.

OPEN – CLOSE – OPEN without the M1 Electrical Motor or with the M1 Electrical Motor Not Energized

WARNING
STORED MECHANICAL ENERGY
  • Prior to withdrawing a circuit breaker without an electrical charging motor from the compartment, use the circuit breaker push buttons to perform a manual OPEN - CLOSE - OPEN operation to discharge the stored energy in the mechanism.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Manually charging the closing springs after the circuit breaker is closed (I CLOSED) will create the initial state of the circuit breaker shown below. From this initial state, the circuit breaker mechanism can perform an OPEN-CLOSE-OPEN operation sequence. The sequence speed is defined according to the application of the customer and is controlled manually or by the protection, control, and monitoring system.

Initial state of the circuit breaker:

 

Perform an OPEN - CLOSE - OPEN operation sequence using either the opening (O OPEN) and closing (I CLOSE) push buttons on the circuit breaker or the electrical controls.

The circuit breaker state indicators will move in the following sequence:

After the first open (O OPEN) operation of the circuit breaker
After the close (I CLOSE) operation of the circuit breaker
After the second open (O OPEN) operation of the circuit breaker

OPEN – CLOSE – OPEN with the M1 Electrical Motor Energized

WARNING
STORED MECHANICAL ENERGY
  • Prior to withdrawing a circuit breaker with an electrical charging motor from the compartment, first disconnect the circuit breaker secondary disconnect plug from the compartment secondary disconnect receptacle. Then use the circuit breaker push buttons to perform a manual OPEN - CLOSE - OPEN operation to discharge the stored energy in the mechanism.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

From the initial state of the circuit breaker shown below, the circuit breaker mechanism can perform an OPEN-CLOSE-OPEN operation sequence without any manual operation on the charging mechanism. The sequence speed is defined according to the application of the customer and is controlled manually by the protection, control, and monitoring system.

Initial state of the circuit breaker:

 

Perform an OPEN - CLOSE - OPEN operation sequence using either the opening (O OPEN) and closing (I CLOSE) push buttons on the circuit breaker or the electrical controls.

The circuit breaker state indicators will move in the following sequence:

Push the open (O OPEN) push button: the circuit breaker opens and the spring-charged state indicator remains charged with the indicator showing "Charged OK".

< 7 seconds later

Push the close (I CLOSE) push button: the circuit breaker closes and the spring-charged state indicator changes to "Discharged" until the electrical motor recharges the spring. The indicator then changes to "Charged OK".
Push the open (O OPEN) push button: the circuit breaker opens and the spring-charged state indicator remains charged with the indicator showing "Charged OK".

Understanding the Racking Mechanism Controls and Indicators

The Racking Mechanism Indicators

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Make sure the entire racking position indicator symbol for the test / disconnected position is visible and centered in the window cutout on the circuit breaker racking mechanism beam to set the circuit breaker in disconnected position.
  • Make sure the entire racking position indicator symbol for the connected position is visible and centered in the window cutout on the circuit breaker racking mechanism beam to set the circuit breaker in connected position.
Failure to follow these instructions will result in death or serious injury.
     

Racking Position Indicator

Circuit Breaker Position

Position Description

Command Available

Connected

The circuit breaker primary contacts are connected to the switchgear primary contacts, the secondary disconnect plug for circuit breaker power and control is connected, and the circuit breaker compartment door should be closed and properly latched.

Transport

The circuit breaker is moving from the disconnected position to the connected position or vice versa. The circuit breaker compartment door should be closed and properly latched. An opening order is maintained during racking in/out operation.

Test/Disconnected

The circuit breaker is inside the circuit breaker compartment, its primary contacts are separated from the switchgear primary contacts by metallic shutters, and the secondary disconnect plug for circuit breaker power and control is disconnected automatically, but it is possible to open the compartment door and move the secondary disconnect plug into the test/disconnected position to connect for testing.

Withdrawn (Removed)

The circuit breaker is extracted from the switchgear using the lift truck.

 

The following table describes the functions available on the EvoPacT circuit breaker within the circuit breaker compartment. For further details, refer to the user guides for the switchgear.

 

Circuit Breaker positions

 

Parts

Connected

Transport

Test/Disconnected

Removed/Withdrawn

Locking tabs

Locked

Locked

Locked / Unlocked

Unlocked

Secondary disconnect plug for circuit breaker power and control

Connected

Connected / Disconnected*

Connected / Disconnected

Disconnected

Low voltage plug for additional features

Connected

Connected

Connected

Disconnected

Compartment door*

Closed

Closed

Closed/Open*

Closed/Open*

Circuit breaker main vacuum bottle position

Open / Closed

Open

Open / Closed

Open*

Circuit breaker compartment racking padlock and keylock (optional)

Padlock install / key removal not possible

Padlock install / key removal not possible

Padlock install and/or key removal possible to allow lockout

Padlock install and/or key removal possible to allow lockout

Shutters

Open

Operating*

Closed

Closed

Red Racking/Emergency Trip Push Button

The red racking/emergency trip push button of the racking mechanism allows:

P

tripping the circuit breaker if the circuit breaker is not in the open (O OPEN) position

O

clearing the access to the racking port

   

The three positions of the red racking/emergency trip push button are:

P1

Pushed-in position: occurs while the button is pushed or while the circuit breaker racking/charging handle is inserted in the racking hole on the racking mechanism. In this position, a limit switch in the breaker assembly is activated to indicate that a manual racking operation may be ongoing. This limit switch is required for the racking mechanism motor interlocking circuit.

P2

Neutral rest position

P3

Pulled-out position: occurs while the button is pulled out and when padlocking is applied to the red push button to prevent opening the circuit breaker racking/charging handle insertion hole on the racking mechanism (see Locking the Racking Mechanism Red Racking/Emergency Trip Push Button).

In this position, a limit switch in the breaker assembly is activated to indicate that a locking condition is present. This limit switch is required for the racking mechanism motor interlocking circuit.

NOTE: The primary contacts on the circuit breaker may be in a welded condition if while pushing the red racking/emergency trip push button, the button does not push in completely and access to the racking port is blocked.

Operation of Locking Tabs

The locking tabs allow the locking of the circuit breaker inside the circuit breaker compartment.

In the normal operation position (without any manual action on the locking handles), the locking tabs are out.

To unlock the circuit breaker, manually push the locking handles to retract the locking tabs.

When the circuit breaker is in the transport or connected positions, the locking tabs are blocked and cannot be operated.

NOTE: Do not try to force the locking handles in if the circuit breaker is not fully racked out into the test/disconnected position.

Motorized Racking Mechanism (Optional)

The racking-in and racking-out operations can be done manually using the genuine Square D™ brand circuit breaker racking/charging handle supplied by Schneider Electric or remotely if the racking mechanism is equipped with a motor option.

The motor is mounted at the rear of the circuit breaker racking mechanism and it is electrically connected to switchgear low voltage instrumentation and controls via the low voltage plug for additional features on the circuit breaker.

The racking motor is a DC permanent magnet machine and it racks the circuit breaker in toward the connected position if the positive side of its power supply is connected to its red lead and racks the circuit breaker out towards the test/disconnected position if the positive side of its power supply is connected to its black lead.

Electrical limit switches are provided within the circuit breaker assembly to provide indication of the breaker position and of the locking status of the emergency trip pushbutton. Refer to Motorized Racking Mechanism Option — Electrical Schematic, in this user guide, for further information.

NOTE: The circuit breaker may still be racked manually when equipped with the motor.

Secondary Disconnect Plug for Circuit Breaker Power and
Control — Operation and Testing the Circuit Breaker in the Test/Disconnected Position

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS or CSA Z462 or local equivalent.
Failure to follow these instructions will result in death or serious injury.

The secondary disconnect plug for circuit breaker power and control, located on the center, top of the circuit breaker:

  • automatically connects with the secondary disconnect receptacle in the circuit breaker compartment when the circuit breaker is racked in and reaches the connected position.

  • automatically disconnects from the secondary disconnect receptacle in the circuit breaker compartment when the circuit breaker is racked out of the connected position towards the test/disconnected position.

  • may not be disconnected from the circuit breaker compartment secondary disconnect receptacle when the circuit breaker is in the connected position.

  • may be connected to the circuit breaker compartment secondary receptacle when the circuit breaker is in the test/disconnected position, providing a convenient method to test the circuit breaker electrical control.

NOTE: The secondary disconnect power and control receptacle in the circuit breaker compartment should remain latched, at the back of its travel in the location where it connects with the circuit breaker in the racked-in, connected position (see Typical Circuit Breaker Compartment Secondary Disconnect Receptacle Assembly and refer to the Schneider Electric document NNZ9886800, SureSeT™ Switchgear User Guide for further information).

To test the circuit breaker in the test/disconnected position:

  1. With the circuit breaker compartment door open, locate the handle attached to the secondary disconnect power and control receptacle (see Typical Circuit Breaker Compartment Secondary Disconnect Receptacle Assembly). It is above the circuit breaker in the circuit breaker compartment.

  2. Rotate the handle downward, in a clockwise direction to an angle of approximately 60–90 degrees.

  3. Pull the handle of the top secondary disconnect receptacle forward until it mates with the secondary disconnect plug on the circuit breaker. The circuit breaker can now be electrically operated in the same way it can when in the connected position.

    NOTE: If the control circuit is energized and the closing spring is discharged, this connection immediately activates the spring charging motor inside the circuit breaker.

  4. Push the close (I CLOSE) push button. If the spring charging motor was correctly activated by the control circuit, the close (I CLOSE) push button should release the closing latch, allowing the closing spring assembly to discharge. The closing spring assembly operates the mechanism which is connected to the vacuum interrupters, and closes the vacuum interrupter contacts. The spring charge motor M1 should start and recharge the closing spring assembly immediately after the closing operation.

  5. Push the open (O OPEN) push button. If the opening spring assembly was correctly charged (compressed) by the closing operation, the mechanism will release the opening latch and allow the opening spring assembly to discharge. The opening spring assembly operates the mechanism which is connected to the vacuum interrupters, which opens the vacuum interrupter contacts.

  6. In this position, it is possible to verify the circuit breaker electrical controls and indications such as the opening and closing releases, spring charge, breaker auxiliary contact status, and ready to close indication. After all the required checks are completed, manually push the receptacle back to its service position using the secondary disconnect receptacle handle. As the secondary disconnect receptacle is moved backwards, allow the handle to rotate clockwise while continuing to push the handle until feeling it snap into the latched position. The secondary disconnect receptacle should be put into this position before racking circuit breakers into the connected position to allow closing of the circuit breaker compartment door prior to the racking operation.

Typical Circuit Breaker Compartment Secondary Disconnect Receptacle Assembly

Circuit breaker compartment secondary disconnect label

Instruction label

Guide pin

Secondary disconnect receptacle handle

Secondary disconnect receptacle for circuit breaker power and control

   
NOTE: When not used for testing the circuit breaker in the test position, the receptacle should remain latched, at the back of its travel in the location where it connects with the circuit breaker plug in the racked-in, connected position. If the receptacle is not in the latched position, then the handle should be used to manually push the receptacle back to the latched, circuit breaker racked-in position before the circuit breaker is racked-in.

Compartment Rating Code Plate

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Make sure the correct circuit breaker has been installed in the correct compartment.
Failure to follow these instructions will result in death or serious injury.

Since the circuit breaker and compartment are equipped with rating code plates, a circuit breaker can not be inserted into the compartment if it does not meet the rated performance of the compartment. To help ensure the circuit breaker is installed into the proper circuit breaker compartment, Schneider Electric recommends:

  • checking the customer order drawings

  • verifying the rating nameplates on the circuit breaker match the rated performance of the circuit breaker compartment

  • verifying the secondary disconnect labels on the circuit breaker align with the labels on the circuit breaker compartment

The compartment rating code plate, constructed of heavy gauge metal, blocks the insertion of a circuit breaker that does not correspond to the compartment. It is mounted on the lower, rear area of the circuit breaker next to the sliding ground contact (see Typical EvoPacT Circuit Breaker Features).

Insertion into and Removal from the Switchgear

DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, or CSA Z462 or local equivalent.
  • Perform all insertions and removals of the circuit breaker with the entire switchgear line-up de-energized.
  • Ensure the left and right lifting eyes on the sides of the circuit breaker have been removed (if the circuit breaker did not come installed in the switchgear).
  • Verify the nameplate data is compatible with that of the electrical installation.
  • Verify the circuit breaker is installed into the proper circuit breaker compartment by checking the customer order drawings and the nameplates, comparing the secondary disconnect labels on the circuit breaker and the circuit breaker compartment, and checking the mimic diagram (if equipped) on the front of the section.
  • Check the correct operation of the MX, XF, and MN auxiliary releases.
Failure to follow these instructions will result in death or serious injury.
WARNING
LIFT TRUCK TIPPING
Use only a SureSeT lift truck to insert and remove the EvoPacT MV circuit breaker into / from SureSeT switchgear.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

To enable circuit breaker removal from or insertion into the switchgear circuit breaker compartment during the installation or maintenance phases, Schneider Electric recommends the use of a lift truck designed to carry the circuit breaker, lock in position at the different insertion points, and adapt to the specific equipment configuration. Circuit breakers used in Schneider Electric SureSeT Switchgear must use its dedicated lift truck manufactured by Schneider Electric. Refer to Schneider Electric user guide NNZ9886800, SureSeT™ MV Metal-Clad, Indoor Switchgear, for further information on obtaining or using the SureSeT lift truck to remove the circuit breaker from or insert it into the circuit breaker compartment.

Manual Racking In

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, or CSA Z462 or local equivalent.
  • Always keep the circuit breaker compartment door closed when racking the circuit breaker from one position to another.
  • Verify the nameplate data is compatible with that of the electrical installation.
  • Verify the circuit breaker is installed into the proper circuit breaker compartment by checking the customer order drawings and the nameplates, comparing the secondary disconnect labels on the circuit breaker and the circuit breaker compartment, and checking the mimic diagram (if equipped) on the front of the section.
Failure to follow these instructions will result in death or serious injury.
WARNING
EXCESSIVE FORCE APPLIED TO EQUIPMENT
Never force the circuit breaker into the circuit breaker compartment. If a racking mechanism is not operating easily, inspect the equipment and remove any foreign objects or debris from inside the circuit breaker compartment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
INAPPROPRIATE RACKING/CHARGING HANDLE useage
  • Only operate the racking mechanism with a genuine Schneider Electric racking/charging handle.
  • Do not attempt to insert the circuit breaker racking/charging handle into the racking mechanism racking hole while the motor of the racking mechanism is operating.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
EXCESSIVE ROTATION SPEED
For a motorized racking mechanism, do not exceed 120 rev/min when racking in or racking out the circuit breaker in manual mode.
Failure to follow these instructions can result in equipment damage.

Perform the following steps to manually rack in the circuit breaker:

  1. Check the customer order drawings and the nameplates on the circuit breaker compartment to verify the circuit breaker is installed in the proper circuit breaker compartment.

  2. Verify the racking position indicator label displays the symbol for the “test/disconnected” position.

  3. If there is a padlock on the red racking/emergency trip push button of the racking mechanism, remove it.

  4. Open the circuit breaker compartment door. Electrically or mechanically open the circuit breaker and if there is a lock-out / tag-out padlock on the circuit breaker compartment, remove it and unlock the key lock (if equipped) to allow racking. (Refer to Schneider Electric user guide NNZ9886800EN, SureSeT™ MV Metal-Clad, Indoor Switchgear, for further information.)

  5. Verify the secondary disconnect plug for circuit breaker power and control is in its service position. If it is not, move it back to the service position. (Refer to Secondary Disconnect Plug for Circuit Breaker Power and
    Control — Operation and Testing the Circuit Breaker in the Test/Disconnected Position
    for further information.)

  6. Close and properly latch the circuit breaker compartment door per the switchgear instructions.

  7. If there is an electromagnet interlock with the racking mechanism, ensure it is energized to allow the racking operation.

  8. Push and hold the red racking/emergency trip push button on the racking mechanism to free the hole for racking handle insertion, then insert the racking/charging handle.

    NOTE: In case the circuit breaker is in the closed (I CLOSED) position, pushing the red racking/emergency trip push button will result in a circuit breaker opening operation. This action will also prevent the racking motor from starting on circuit breakers equipped with motorized racking systems.
    NOTE: The racking mechanism must be properly and fully latched into the breaker compartment with both left and right locking tabs fully extended into the latch plates on the rails in the circuit breaker compartment in order to open the racking port.
  9. Rotate the racking/charging handle clockwise until the racking mechanism state indicator moves to the connected position, as shown below.

    NOTE: When the racking position indicator symbol displays the image for “connected,” the circuit breaker is fully racked into the circuit breaker compartment and the primary contacts of the circuit breaker are connected.
    NOTE: Interlocks, integrated into the circuit breaker, ensure the circuit breaker primary contacts are in the open (O OPEN) position prior to moving the circuit breaker from the connected or test/disconnected position and ensure the circuit breaker primary contacts remain open (O OPEN) while the circuit breaker is moving in the transport position.

    Circuit Breaker Stroke Number of Racking/Charging Handle Turns
    9.875 in. / 250.8 mm 41
  10. Remove the racking/charging handle. The circuit breaker is now in the "connected" position and can either be operated for normal service or racked back to the test/disconnected position (refer to Understanding the Racking Mechanism Controls and Indicators for further information).

    NOTE: The racking/charging handle can be extracted from the racking port at any time prior to the end of the racking in operation, but this action stops the operation. Operation can be resumed by reinserting the racking/charging handle after pushing and holding the red racking/emergency trip push button on the racking mechanism.

Manual Racking Out

DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, or CSA Z462 or local equivalent.
  • Always keep the circuit breaker compartment door closed when racking the circuit breaker from one position to another.
Failure to follow these instructions will result in death or serious injury.
WARNING
EXCESSIVE FORCE APPLIED TO EQUIPMENT
Never force the circuit breaker out of the circuit breaker compartment. If a racking mechanism is not operating easily, inspect the equipment and remove any foreign objects or debris from inside the circuit breaker compartment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
INAPPROPRIATE RACKING/CHARGING HANDLE Useage
  • Only operate the racking mechanism with a genuine Schneider Electric racking/charging handle.
  • Do not attempt to insert the circuit breaker racking/charging handle into the racking mechanism racking hole while the motor of the racking mechanism is operating.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
EXCESSIVE ROTATION SPEED
For a motorized racking mechanism, don’t exceed 120 rev/min when racking in or racking out the circuit breaker in manual mode.
Failure to follow these instructions can result in equipment damage.


Perform the following steps to manually rack out the circuit breaker:

  1. Verify the racking position indicator label displays the symbol for the “connected” position.

  2. Ensure the circuit breaker compartment door is closed and properly latched per the switchgear instructions.

  3. If there is a padlock on the red racking/emergency trip push button of the racking mechanism, remove it.

  4. If the circuit breaker is in the closed (I CLOSED) position, electrically open it.

  5. If there is an electromagnet interlock with the racking mechanism, ensure it is energized to allow the racking operation.

  6. Push and hold the red racking/emergency trip push button on the racking mechanism to free the hole for racking handle insertion, then insert the racking/charging handle.

    NOTE: In case the circuit breaker is in the closed (I CLOSED) position, pushing the red racking/emergency trip push button will result in a circuit breaker opening operation. This action will also prevent the racking motor from starting on circuit breakers equipped with motorized racking systems.
  7. Rotate the racking/charging handle counter-clockwise until the racking mechanism state indicator moves to the Test/Disconnected position, as shown below.

    NOTE: When the racking position indicator symbol displays the image for “test/disconnected,” the circuit breaker is fully racked out in the circuit breaker compartment and the primary high voltage contacts of the circuit breaker are disconnected.
    NOTE: Interlocks, integrated into the circuit breaker, ensure the circuit breaker primary contacts are in the open (O OPEN) position prior to moving the circuit breaker from the connected or test/disconnected position and ensure the circuit breaker primary contacts remain open (O OPEN) while the circuit breaker is moving in the transport position.

    Circuit Breaker Stroke Number of Racking/Charging Handle Turns
    9.875 in. / 250.8 mm 41
  8. Remove the racking/charging handle. The circuit breaker is now in the "test/disconnected" position and can either be operated for test operations, withdrawn from the circuit breaker compartment, or racked back into the connected position (refer to Understanding the Racking Mechanism Controls and Indicators for further information).

    NOTE: The racking/charging handle can be extracted from the racking port at any time prior to the end of the racking out operation, but this action stops the operation. Operation can be resumed by reinserting the racking/charging handle after pushing and holding the red racking/emergency trip push button on the racking mechanism.

Remote Racking In

DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS, or CSA Z462 or local equivalent.
  • Always keep the circuit breaker compartment door closed when racking the circuit breaker from one position to another.
  • Verify the nameplate data is compatible with that of the electrical installation.
  • Verify the circuit breaker is installed into the proper circuit breaker compartment by checking the customer order drawings and the nameplates, comparing the secondary disconnect labels on the circuit breaker and the circuit breaker compartment, and checking the mimic diagram (if equipped) on the front of the section.
  • It is responsibility of the switchgear manufacturer to ensure that proper interlocking is applied to the circuit breaker racking mechanism motor control circuit.
Failure to follow these instructions will result in death or serious injury.
CAUTION
UNEXPECTED EQUIPMENT OPERATION
  • Remove the racking/charging handle to allow racking in / racking out operations with racking mechanism motor control.
  • Do not attempt to insert the circuit breaker racking/charging handle into the racking mechanism racking hole while the motor of the racking mechanism is operating.
Failure to follow these instructions can result in injury or equipment damage.

Rack-in operations may be performed electrically in circuit breakers equipped with an optional racking mechanism motor.

The control circuit of the circuit breaker racking mechanism motor is located in the switchgear control cabinet and may differ according to the switchgear type and its manufacturer. Indication contacts are provided within the circuit breaker assembly and connected to the LV plug for additional features to be used in the racking motor control circuit that shall provide start, stop, motor protection, and interlocking functions.

It is responsibility of the switchgear manufacturer to ensure that proper interlocking is applied to the racking mechanism motor.

The following interlocking condition must be provided as a minimum:

  • The racking mechanism motor operation is prevented unless the circuit breaker is in the open (O OPEN) position.

  • The racking mechanism motor operation is prevented in case a manual operation is ongoing or the racking/charging handle is inserted in its port.

  • The racking mechanism motor operation is prevented in case a locking condition (such as key lock or padlock activation) is applied.

  • In case the racking mechanism locking electromagnet is supplied, the racking mechanism motor operation is prevented in case the magnet is not powered on. The electromagnet indication contact shall be used for this interlocking function.

  • Power to the racking mechanism motor is shut down if a peak current or time of transport is exceeded in cases where an object is impeding the racking.

    NOTE: If this situation occurs, inspect the equipment for correct functionality and/or remove any foreign objects or debris from inside the circuit breaker compartment.

Perform the following steps to remotely rack in the circuit breaker:

  1. Check the customer order drawings and the nameplates on the circuit breaker compartment to verify the circuit breaker is installed in the proper circuit breaker compartment.

  2. Verify the racking position indicator label displays the symbol for the “test/ disconnected” position.

  3. If there is a padlock on the red racking/emergency trip push button of the racking mechanism, remove it.

  4. Open the circuit breaker compartment door. Electrically or mechanically open the circuit breaker and if there is a lock-out / tag-out padlock on the circuit breaker compartment, remove it and unlock the key lock (if equipped) to allow racking. (Refer to Schneider Electric user guide NNZ9886800EN, SureSeT™ MV Metal-Clad, Indoor Switchgear, for further information.)

  5. Verify the secondary disconnect plug for circuit breaker power and control is in its service position. If it is not, move it back to the service position. (Refer to Secondary Disconnect Plug for Circuit Breaker Power and
    Control — Operation and Testing the Circuit Breaker in the Test/Disconnected Position
    for further information.)

  6. Close and properly latch the circuit breaker compartment door per the switchgear instructions.

  7. If there is an electromagnet interlock with the racking mechanism, ensure it is energized to allow the racking operation.

  8. Launch an electrical rack-in operation from the switchgear front panel or via a remote control system. The motor should operate the racking mechanism until the circuit breaker reaches the connected position. The circuit breaker is now in the "connected" position and can either be operated for normal service or racked back to the test/disconnected position (refer to Understanding the Racking Mechanism Controls and Indicators for further information).

    NOTE: When the racking position indicator symbol displays the image for “connected,” the circuit breaker is fully racked into the circuit breaker compartment and the primary high voltage contacts of the circuit breaker are connected.
    NOTE: Interlocks, integrated into the circuit breaker, ensure the circuit breaker primary contacts are in the open (O OPEN) position prior to moving the circuit breaker from the connected or test/disconnected position and ensure the circuit breaker primary contacts remain open (O OPEN) while the circuit breaker is moving in the transport position.
    Circuit Breaker Stroke Duration
    9.875 in. / 250.8 mm < 60 s at rated control voltage

Remote Racking Out

DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462 or local equivalent.
  • Always keep the circuit breaker compartment door closed when racking the circuit breaker from one position to another.
  • It is responsibility of the switchgear manufacturer to ensure that proper interlocking is applied to the circuit breaker racking mechanism motor control circuit.
Failure to follow these instructions will result in death or serious injury.
CAUTION
UNEXPECTED EQUIPMENT OPERATION
  • Remove the racking/charging handle to allow racking in / racking out operations with the racking device motor control.
  • Do not attempt to insert the circuit breaker racking/charging handle into the racking mechanism racking hole while the motor of the racking mechanism is operating.
Failure to follow these instructions can result in injury or equipment damage.

Rack-out operations may be performed electrically in circuit breakers equipped with an optional racking mechanism motor.

The control circuit of the circuit breaker racking mechanism motor is located in the switchgear control cabinet and may differ according to the switchgear type and its manufacturer. Indication contacts are provided within the circuit breaker assembly and connected to the LV plug for additional features to be used in the racking motor control circuit that shall provide start, stop, motor protection, and interlocking functions.

It is responsibility of the switchgear manufacturer to ensure that proper interlocking is applied to the racking mechanism motor.

The following interlocking condition must be provided as a minimum:

  • The racking mechanism motor operation is prevented unless the circuit breaker is in the open (O OPEN) position.

  • The racking mechanism motor operation is prevented in case a manual operation is ongoing or the racking/charging handle is inserted in its port.

  • The racking mechanism motor operation is prevented in case a locking condition (such as key lock or padlock activation) is applied.

  • In case the electromagnetic interlocking of the racking mechanism is supplied, the racking mechanism motor operation is prevented in case the electromagnet is not powered on. The electromagnet indication contact shall be used for this interlocking function.

  • Power to the racking mechanism motor is shut down if a peak current or time of transport is exceeded in cases where an object is impeding the racking.

    NOTE: If this situation occurs, inspect the equipment for correct functionality and/or remove any foreign objects or debris from inside the circuit breaker compartment.

Perform the following steps to remotely rack out the circuit breaker:

  1. Verify the racking position indicator label displays the symbol for the “connected” position.

  2. Ensure the circuit breaker compartment door is closed and properly latched per the switchgear instructions.

  3. If there is a padlock on the red racking/emergency trip push button of the racking mechanism, remove it.

  4. If the circuit breaker is in the closed (I CLOSED) position, electrically open it.

  5. If there is an electromagnet interlock with the racking mechanism, ensure it is energized to allow the racking operation.

  6. Launch an electrical rack-out operation from the switchgear front panel or via a remote control system. The motor should operate the racking mechanism until the circuit breaker reaches the test/disconnected position. The circuit breaker is now in the "test/disconnected" position and can either be operated for test operations, withdrawn from the circuit breaker compartment, or racked back into the connected position (refer to Understanding the Racking Mechanism Controls and Indicators for further information).

    NOTE: When the racking position indicator symbol displays the image for “test/disconnected,” the circuit breaker is fully racked out in the circuit breaker compartment and the primary high voltage contacts of the circuit breaker are disconnected.
    NOTE: Interlocks, integrated into the circuit breaker, ensure the circuit breaker primary contacts are in the open (O OPEN) position prior to moving the circuit breaker from the connected or test/disconnected position and ensure the circuit breaker primary contacts remain open (O OPEN) while the circuit breaker is moving in the transport position.
    Circuit Breaker Stroke Duration
    9.875 in. / 250.8 mm < 60 s at rated control voltage

Locking the Racking Mechanism Controls

Electromagnetic Interlocking of the Racking Mechanism

Manual and electrical circuit breaker racking operations may be prevented if the optional electromagnetic interlock of the racking mechanism is provided.

The electromagnet assembly is composed of an electromechanical coil, mechanical linkages, and an indication contact that is closed when the coil is energized and open when the coil is not energized. The assembly for the electromagnetic interlocking of the racking mechanism is located on the bottom left side of the mechanism area (see the figure Circuit Breaker Mechanism Area).

When the electromagnet is energized, the red racking/emergency trip push button may be pushed allowing a manual racking operation. When the electromagnet is not energized the red racking/emergency trip push button cannot be pushed, so a manual racking operation may not be performed.

Electrical racking is prevented by the usage of the electromagnet assembly indication contact which shall be used in the racking mechanism motor control circuit in the LV cabinet to prevent the racking motor from running if the electromagnet is not energized.

Locked

When the coil is NOT energized:
  • the red racking/emergency trip push button is blocked, preventing pushing it.

  • the hole for racking handle insertion is blocked, preventing insertion of the racking/charging handle.

  • no manual or electrical racking in or out of the circuit breaker is permitted.

  Unlocked

When the coil is energized:

  • the red racking/emergency trip push button is not blocked

  • the hole for racking handle insertion can open

  • normal racking of the circuit breaker is permitted

Locking the Racking Mechanism Red Racking/Emergency Trip Push Button

DANGER
hazard of electric shock, explosion, or arc flash
  • Always practice lock-out/tag-out procedures according to OSHA requirements. Use out-of-service tags and padlocks when working on equipment. Leave tags in place until the work is completed and the equipment is ready to be put back into service.
  • Do not use locking the red racking/emergency trip push button as a means to lock-out/tag-out a circuit breaker compartment.
  • The switchgear manufacturer must wire the controls properly to interlock electrical motorized racking with the locking of the racking mechanism red racking/emergency trip push button.
Failure to follow these instructions will result in death or serious injury.

The racking mechanism can be locked in the connected or test/disconnected position by pulling out the red racking/emergency trip push button and then placing a padlock or a multiple locking hasp system, with one or several padlocks, in the provided hole. Padlocks or lockout hasps are not supplied.

NOTE: In this application, padlocks only block the racking mechanism on the circuit breaker. Padlocking the red racking/emergency trip push button does not properly lock-out/tag-out a circuit breaker compartment due to the integrated nature of the racking device on the circuit breaker. To properly lock-out/tag-out a circuit breaker compartment, a lock-out/tag-out system on the circuit breaker compartment must be properly applied.

When the red racking/emergency trip push button is locked:

  • manual racking in or racking out is not possible

  • electrical racking in or racking out is not possible (provided the racking motor control circuit on the switchgear is properly designed)

  • emergency tripping of the circuit breaker is not possible using this push button

    NOTE: the circuit breaker may still be opened using the open (O OPEN) push button on the front of the circuit breaker
  • electrical opening of the circuit breaker is still possible

  • in the test/disconnected position, removal of the circuit breaker is still possible

Lock

Pull-out the red racking/emergency trip push button and padlock it.

 

Check

The red racking/emergency trip push button is blocked.

 

Unlock

Remove the padlock(s) to release the red racking/emergency trip push button.

Locking the Circuit Breaker in the Test/Disconnected Position in SureSeT Switchgear

When a padlock or key lock is used in the circuit breaker compartment for lock-out/tag-out proceedures (not using the red racking/emergency trip push button), the racking mechanism is blocked from operating and the circuit breaker is unable to move into the connected position. However, the circuit breaker can be removed from the compartment if necessary. Refer to Schneider Electric user guide No NNZ9886800EN, SureSeT™ MV Metal-Clad, Indoor Switchgear, for further information.

Protection, Control, and Monitoring

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Never close a circuit breaker connected to the main power circuit unless the tripping chain voltage is energized and the protection, control, and monitoring controllers are connected and operable.
Failure to follow these instructions will result in death or serious injury.

To enable assisting the electrical protection of the installations, the EvoPacT circuit breaker must be coupled with a protection, control, and monitoring system installed in the switchgear that houses the circuit breaker.

Refer to the switchgear factory drawings and user guide.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.