JYT3013100

Introduction to EvoPacT

Presentation of the Medium Voltage Vacuum Circuit Breaker (VCB)

Function

The Square D™ brand EvoPacT medium voltage vacuum circuit breaker is a drawout (removable) device enabling switching and assists in the protection of distribution networks. Installed in medium voltage switchgear used up to 15 kV, it provides up to 40 kA short circuit interrupting capability protecting downstream conductors and limiting the electrical and mechanical stress to components situated downstream. The specific rating of each circuit breaker is printed on the circuit breaker nameplate. The EvoPacT medium voltage circuit breaker is a horizontal drawout circuit breaker designed for use with medium voltage metal-clad switchgear.

Surge Protection for EvoPacT Circuit Breakers (Statement of Use)

Circuits in which these circuit breakers are placed are capable of producing overvoltages. The following general guidelines will address the vast majority of application concerns. However, they do not guarantee complete system protection from the occurrence of overvoltages.

  • Complex medium voltage systems may require a detailed overvoltage system analysis and the addition of an RC network.

  • All circuits should have at least distribution class arresters unless cable lengths exceed 300 ft. (91.5 m). In many cases, external arresters are already used for other reasons. Surge protection is not provided as standard equipment, but is an available option (as necessary per customer specifications).

  • For dry-type (including cast-resin type) transformers and motor loads, surge capacitors should be used at the terminals of the transformer or motor. Where there are long lengths of cable, the cable capacitance may offer surge capacitor protection if the cable capacitance is equivalent to typical values available in surge capacitors.

Nameplate

The nameplate shown here is only to be used as an example and does not reflect actual values that will be stated on the customer specific circuit breaker nameplate. The customer’s specific circuit breaker ratings and all required information will be shown on the nameplate of the circuit breaker. The nameplate label also shows information on the motors and auxiliary control units installed on the device, and their operating voltages. The nameplate label is placed near the center of the circuit breaker front cover.

How to Use the Nameplate QR Code

The serial number (SN) located on the nameplate is using 18 characters in order to be easy to understand. Example: SE-2016-W44-5-0018.

To access to Safe Repository, enter the serial number with its simplified 11 characters’ format. Example: SE164450018.

If the long description is typed in, it will be automatically converted to the short description. The QR code link implement the simplified format.

The QR code, located on the nameplate, grants access from a smartphone or a connected tablet to all data relating to the specific circuit breaker including:

  • serial number

  • operating characteristics

  • user guide

  • warranty period

To access this information, read the QR code with a smartphone or connected tablet. The QR code will open a website containing the data relating to the circuit breaker. Follow the website instructions to obtain personal access.

The serial number and the commercial reference number also allow access to the information without a smartphone or connected tablet.

Typical EvoPacT Circuit Breaker Features

(15 kV, 2000 A, 40 kA shown)

       
  A

Primary high voltage contacts (runbacks and clusters)

B

Secondary disconnect plug and cover for circuit breaker power and control

C

Front cover

D

Circuit breaker nameplate

E

Push buttons and indicators

E1

Opening pushbutton (red with white "O OPEN")

E2

Closing pushbutton (black with white "I CLOSE")

E3

Mechanical operation counter

E4

Spring charged status indicator

E5

Main contact position indicator

F

Insertion opening for manual charging of the operating mechanism

G

Operating instructions

H

Shutter operating ramps

I

Racking mechanism beam green locking handles

J

Racking position indicator

K

Insertion opening for manual racking of the racking mechanism

L

Red racking/emergency trip push button

M

Locking tabs

N

Roll on the floor wheels

O

Positioning rail wheels

P

Lift truck manual latch hoist hook slots

Q

Pull handle

R

TOC pin

S

Automatic discharge pin

T

MOC mechanism (optional)

NOTE: Items identified on this page may be named in table continued on the next page. Items may also be identified in images on both this page and the next page.
  U

TH110 sensors location*

  V

Vacuum bottle interrupter contact monitoring erosion gap (E-gap) sensors location*

W

Breaker mechanism operating closing and opening speed monitoring sensor not visible behind front cover. Refer to Circuit Breaker Mechanism Area.*

X

Lifting bracket (when equipped/removable)

Y

Shipping bracket (when equipped/removable)

Z

Racking mechanism motor (optional)

AA

Padlockable racking/trip push button shielding location (shielding assembly not shown) (optional)

BB

Motorized Racking Truck Label (when equipped with racking mechanism motor)

  CC Low voltage plug for additional features
  DD Sliding ground contact
  EE

Vacuum bottle interrupters (VI’s)

  FF

Racking mechanism

  GG

Compartment rating code plate

 
NOTE: Items identified on this page may be named in table continued from the previous page. Items may also be identified in images on both this page and the previous page.
 

Operating Instruction Labels

This label, located on the front cover, shows how local manual controls are used (switching between open (O OPEN) and closed (I CLOSED) states and manual spring charging).

Circuit Breaker Operating Instructions


These labels, located on the door of SureSeT switchgear circuit breaker compartments, provide a pictorial guide to the manual racking in/out operations. These labels are specific to the customer's switchgear equipment. Refer to the switchgear user guide for further information.

Circuit Breaker Manual Racking Operating Instructions


NOTE: These labels are not provided on the EvoPacT circuit breaker.

Service Conditions

Normal Service Conditions

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS,  CSA Z462, or local equivalent.
  • Observe all circuit breaker installation, operation, and usage instructions.
  • Never operate the circuit breaker if it is damaged.
  • Do not allow the ambient operating temperatures to exceed the specified limits.
  • The ambient operating air must not be significantly polluted by dust, particulates, smoke, corrosive and/or flammable gases, vapors, or salt.
Failure to follow these instructions will result in death or serious injury.

The circuit breaker, including its auxiliary and control circuits, is designed to operate according to its rated characteristics and the service conditions below:

Operating Characteristics of the EvoPacT Circuit Breaker in SureSeT Switchgear

Characteristic

Indoor Switchgear

Ambient Air Temperature

Ideal value

Minimum value

Maximum value

Average measured over a 24-hour period

70°F (21°C)

23°F (-5°C)

104°F (40°C)

≤ 95°F (35°C)

Average Relative Humidity

Ideal value

Measured over a 24-hour period

Measured over a 1-month period

≤ 75%

≤ 95%

≤ 90%

Average Water Vapor Pressure

Measured over a 24-hour period

Measured over a 1-month period

≤ 2.2 kPa

≤ 1.8 kPa

Altitude Above Sea Level

≤ 3300 ft. (1000 m)

Atmosphere

The ambient air should be clean and must not be significantly polluted by dust, particulates, smoke, corrosive and/or flammable gases, vapors, or salt, and no condensation.

Other Service Conditions

If operated beyond the normal service conditions, the circuit breaker is submitted to accelerated aging.

The circuit breaker may only be used under conditions other than the normal service conditions with express written permission from Schneider Electric.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.