JYT3013100

Overall Information

Before Beginning

  • This user guide is meant for a qualified person who will transport, store, handle, receive, install, operate, service, and maintain the circuit breaker: i.e. equipment manufacturers, installers, end users, etc. The generic term used in this guide for any such person is “user”.

  • This user guide cannot be used to define or check the compatibility of the equipment with every single user application, nor its reliability within it. It is the duty of every user to perform a complete risk analysis, evaluation, and testing of the products in specific applications in accordance with applicable standards.

  • When the products are used in applications with specific technical requirements, the integration and protection rules for the specific application must be followed.

  • It is the duty of every user to ensure the device is used within the environment and mission profile stated in this user guide. The environment in which this circuit breaker was designed to be stored, installed, and operated is specified throughout this user guide.

Purpose of the Document

This user guide is an integral part of the equipment. It describes the operation and use of the 5/15 kV EvoPacT™ Medium Voltage Vacuum Circuit Breaker manufactured by Square D of Schneider Electric, as well as its storage, handling, installation, and maintenance instructions. This document must be available at any time to the qualified personnel required to use or work on the circuit breaker. If the equipment is sold after installation, this document must be given to the new owner.

Please read this user guide carefully and follow its recommendations. However, the user guide cannot describe every single condition of use or every variant specific to the customer.

Access to the Technical Documentation

Visit our website www.se.com for:

  • downloading additional documents.

  • contacting Schneider Electric customer support for necessary information not contained in this document.

  • any suggestions on how to improve this document.

Connect to https://alm.se.com/console/ and enter the reference number and the serial number of the circuit breaker to download:

  • “public documents” regarding EvoPacT.

  • “private documents” specific to the equipment.

Access this information by using the QR code located on the front cover of the circuit breaker.

Referenced User Guides

For each device or system referenced in this user guide, there is a corresponding user guide available. Each user guide describes the safety information, features, receiving/handling/storage instructions, operation, use, and maintenance procedures of the corresponding MV device.

NOTE: Access any of the user guides shown in the table by clicking the document number.

NNZ9886800

QGH51397*

NVE62740

P5/EN M/44B

NRJCAT17764EN

GEX2048200

Limitation of Liability

Schneider Electric cannot be held responsible for damage due to :

  • failure to follow the instructions in this guide and additional documents.

  • improper use of the equipment.

  • improper assembly, testing, installation, connection or misuse of the equipment.

  • use of components or spare parts other than the ones recommended by Schneider Electric.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.