JYT3013100

Overview of the Electrical Auxiliaries

Identification of Auxiliary Labels on the Wiring Module

  Symbol Description
  EOS-BM100 Breaker Monitoring Module
  MC110 Mechanism speed sensor
  Y0 Truck blocking magnet
  S3 Truck blocking magnet indication contact
  M2 Not available
  S5 Not available
  VI110 E-gap sensors
  A E-gap sensor phase A connection
  B E-gap sensor phase B connection
  C E-gap sensor phase C connection
  Truck Connections to circuit breaker truck
  M1 Spring charge motor
  MITOP Not available
  MX2/MN Optional trip coil (Second coil or UV coil)
  XF Close coil
  MX1 Trip coil
  S4 Trip signal detection limit switch
  Y1 Close blocking magnet
     

Circuit Breaker Auxiliary Switch

The auxiliary switch is a multi stage switch used to operate circuits that depend on the position of the circuit breaker contacts. It is housed in the wiring module behind the front cover of the circuit breaker and a cover plate. It is located to the upper left of the circuit breaker ARF200 operating mechanism (see Circuit Breaker Mechanism Area). The schematic diagram illustrates how each of the auxiliary switch contacts interconnect with the circuit breaker circuitry (refer to Typical Circuit Breaker Electrical Schematic).

Circuit Breaker Open and Close Coils

DANGER
loss of circuit breaker control
  • Ensure the power connection on release coils is continuously energized.
  • Ensure the power connection on release coils is not connected to the circuit breaker trip/close contact.
  • Ensure the order connection on release coils is connected to the circuit breaker trip/close contact.
  • Ensure the common connection on release coils connects to the negative/grounded side of the release coil power supply.
Failure to follow these instructions will result in death or serious injury.

The opening and closing coils used on the EvoPacT circuit breaker are electronic coils and must be continuously supplied with power for proper operation (refer to Typical Circuit Breaker Electrical Schematic). When energized by the switchgear or remote circuitry, these coils release the open or close latches located inside the mechanism. The standard location of the open and close release coils is mounted on the top center of the ARF200 operating mechanism (see Circuit Breaker Mechanism Area). They feature an integrated electronic circuit board that allows for:

  • self-checking functionality reporting of internal coil failures, such as failure of the electronic board or coil winding continuity.

  • indication of coil activation to report coil activation timing.

  • the use of external trip coil supervision devices.

The standard coil activation connections are wired to the open/close circuits of the switchgear. The additional coil features require the circuit breaker to be configured with particular specifications to permit functionality.

The MX1 opening release coil opens the circuit breaker. The XF closing release coil closes the circuit breaker. An optional MX2 or MN opening release coil to open the circuit breaker can also be specified (refer to Circuit Breaker Equipped With an MN Under-Voltage Opening Release, for further information on the MN release coil). The MX2 opening release coil provides an option for having an additional tripping coil on the circuit breaker ARF200 operating mechanism.

The coils feature five external connections. Three connections are allocated to coil activation and two are for additional features. The three activation connections consist of one “power”, one “order”, and one “common” connection:

  • The power connection is required to be continuously energized and is the power supply of the electronic circuit board of the coil. Ensure that the power connection is not connected to the circuit breaker trip/close contact.

  • The order connection activates the plunger of the coil when energized. Ensure that the order connection is connected to the circuit breaker trip/close contact(s) and, if required, to the trip coil supervision device.

  • The common connection connects to the negative/grounded side of the release coil power supply.

Blocking Magnet for Circuit Breaker Closing

Manual and electrical circuit breaker closing operations may be prevented if the optional circuit breaker closing blocking electromagnet is provided.

The electromagnet assembly is composed of an electromechanical coil and mechanical linkages, and an indication contact that is closed when the coil is energized and open when the coil is not energized (refer to the Typical Circuit Breaker Electrical Schematic for further details). The assembly for the electromagnetic interlocking of the racking mechanism is located on the upper right side of the ARF200 operating mechanism (see Circuit Breaker Mechanism Area).

  • When the electromagnet coil is energized, closing of the circuit breaker is permitted.

  • When the electromagnet coil is not energized, then both mechanical and electrical closing of the circuit breaker is blocked.

Anti-Pump Function

DANGER
ANTI-PUMP loss
The XF closing release must not be wired in series with any of the circuit breaker auxiliary contacts.
Failure to follow these instructions will result in death or serious injury.

The EvoPacT circuit breaker is provided with a mechanical anti-pump function system embedded in its mechanism. The anti-pump system ensures that the closing order that previously caused the circuit breaker to close must be reset in order to allow the circuit breaker to close again. This prevents the breaker from “pumping” in case of a latched close command is mechanically or electrically applied to the circuit breaker.

It is mandatory that auxiliary contacts of the circuit breaker are not wired in series to the closing release (XF) and its close contact in order to prevent defeating the mechanical anti-pump system of the EvoPacT circuit breaker.

NOTE: The EvoPacT XF and MX releases are able to be continuously energized.
NOTE: It is allowed to wire auxiliary contacts of other circuit breakers to the XF closing release order connection for interlocking purposes.

EvoPacT Electrical Diagrams

The information in this section describes the EvoPacT electrical circuit components. The following electrical diagrams show a standard application for the EvoPacT circuit breaker (see Typical Circuit Breaker Electrical Schematic) and racking mechanism (see Motorized Racking Mechanism Option — Electrical Schematic). The electrical circuit designs may vary, depending upon customer requirements, EvoPacT specifications, and switchgear integration.

Typical Circuit Breaker Electrical Schematic

Always refer to the specific circuit breaker schematic diagram in the customer order drawings.

Typical Circuit Breaker Electrical Schematic


NOTE: Information on the operation of the circuit breaker:
  • Operation of coils MX1, MX2, and MN causes the circuit breaker to open.

  • Operation of coil XF causes the circuit breaker to close provided that the ready to close conditions are met. Refer to “Ready to Close” Indication in this user guide, for further information.

  • Coils XF, MX1, MX2 are actuated when:

    1. rated voltage is applied across the “power” terminal and the “common” terminal, And

    2. rated voltage is applied across the “order” terminal and the “common” terminal

    When voltage is applied exclusively across the “power” terminal and the “common” terminal, only the electronic board of the coil is powered up allowing monitoring functions (if equipped) to run, but the coil plunger is not actuated. Coils MX2 and MN are optional and may not be provided.

  • Coil MN operates when the voltage across its terminals is below 70% of its rated value. The coil may reset when the voltage across its terminals is between 70% and 85% of its rated value and it is guaranteed to reset when the voltage across its terminals is above 85% of its rated value. Coil MN is optional and may not be provided.

  • When magnet Y1 (if equipped) is energized, the circuit breaker is allowed to close via an electrical (close coil) or mechanical (push button) command. Removing the power supply to the magnet prevents any closing operations to be performed. It is recommended to wire a normally closed circuit breaker auxiliary contact in series to Y1 in the equipment instrumentation compartment in order to extended the magnet lifespan and to decrease its energy consumption. Magnet Y1 is optional and may not be provided.

  • Anti-pumping function is provided through mechanical features. Wiring circuit breaker auxiliary contacts to the tripping or closing circuit defeats the mechanical antipump system.

  • Switch S2 is shown with closing spring in the charged position.

Motorized Racking Mechanism Option — Electrical Schematic

SDX:

Low voltage plug for additional features

SC1:

Pushing the red racking/emergency trip push button opens the microswitch

SC7:

Pulling of the red racking/emergency trip push button opens the microswitch

XRM:

2–pin motor connector

RM:

Motor for Rack-in/Rack-out

SP1A/SP1B:

Microswitch for Rack-in motor stop

SP2A/SP2B:

Microswitch for Rack-out motor stop

 

SC1:

Open Close Close

SC7:

Close Close Open
NOTE: Microswitch contacts in schematic are shown with:
  • Racking mechanism not under manual operation

  • Racking mechanism red racking/emergency trip push button not padlocked

  • Racking mechanism in transport position. SP1A and SP1B (when equipped) close when breaker is fully racked in, SP2A and SP2B (when equipped) close when the circuit breaker is fully racked out.

NOTE: When magnet Y0 is energized, the circuit breaker is allowed to be racked in or out (mechanically or electrically). Removing the power supply to the magnet prevents from any racking operations to be performed.

Motorized Racking Mechanism Option — Electrical Schematic

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.