Receiving, Handling, and Storage
This section contains instructions for receiving, handling, and storing 5/15 kV EvoPacT Medium Voltage Vacuum Circuit Breakers. Follow all safety precautions before working on the equipment.
Receiving
EvoPacT circuit breakers are shipped wrapped on individual pallets inside protective containers. Do not stack the circuit breakers. The circuit breaker box may have crush cones attached to the top. If the cone is crushed, do not accept or use the circuit breaker and report as potential shipping damage to the freight carrier.
Upon receipt, compare the packing list to the equipment received to make sure the order and shipment are complete. Claims for shortages or errors must be made in writing to Schneider Electric within 60 days of delivery. Failure to give such notice will constitute unqualified acceptance and a waiver of all such claims by the purchaser.
Immediately inspect the equipment for any damage that may have occurred in transit. If damage is found or suspected, do not use the equipment, file a claim with the carrier immediately, and notify Schneider Electric. Delivery of equipment to a carrier at any of the Schneider Electric plants or other shipping point constitutes delivery to the purchaser regardless of freight payment and title. All risk of loss or damage passes to the purchaser at that time.
Handling
WARNING |
|---|
|
FALL OR TIPPING OF THE circuit breaker DURING UNLOADING
OR HANDLING
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
|---|
|
INAPPROPRIATE HANDLING
Failure to follow these instructions can result in injury or equipment damage.
|
Weight
Position of Center of Gravity
How to Lift and Move the Circuit Breaker
|
If the circuit breaker needs to be lifted, for example, when it is shipped on a pallet, please follow the instructions below after unbolting both of the shipping brackets from the pallet and removing any shipping restraints/packaging.
-
When lifting the circuit breaker by a hoist, verify that it is capable of supporting the weight.
-
Lift the circuit breaker using the lifting brackets on the top (left and right side) of the breaker mechanism area.
-
Ensure that the lifting strap is at such an angle to not press on the housing of the outer pole assemblies of the circuit breaker.
-
Use the second hole from the front of the circuit breaker, marked with a “II” symbol below it.
-
Never lift the circuit breaker with a forklift from below.
When maneuvering the circuit breaker, guide the circuit breaker by the green recessed handles of the racking mechanism beam or the pull handle located at the front, middle of the plate covering the racking mechanism.
Do not lift, grasp, or move the circuit breaker by the primary high voltage connections.
Do not push on the front covers or phase insulator barriers of the circuit breaker as it may cause them to break.
The circuit breaker can be moved by rolling on the floor, but do not attempt to move on excessively rough floors, uneven surfaces, or outside ground surfaces.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Remove the shipping and lifting brackets from the circuit
breaker before installing it in the circuit breaker compartment of
the switchgear.
Failure to follow these instructions will result in death or serious injury.
|
Remove the shipping and lifting brackets from the circuit breaker, before installing the circuit breaker in the circuit breaker compartment of the switchgear. Store the lifting brackets and the mounting hardware close to the switchgear line-up operating area.
Storage
If the equipment is stored prior to installation, follow these storage instructions:
Moisture Contamination Avoidance and Mitigation
Safety Precautions
DANGER |
|---|
|
Hazard of Electric Shock, Explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
fire hazard
Remove all flammable material in the vicinity of the heaters,
such as packaging, accessories in boxes, and documentation, before
energizing the heaters.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Shipping, Receiving, and Storage Requirements
This equipment does not achieve its ratings until it is installed per record/as-built drawings, installed per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be stored in a climate controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment is not suitable for outdoor storage.
-
The equipment should be treated as if it is in storage until it is installed and operational. The storage area should be clean, dry (75% or less relative humidity), and climate controlled with proper ventilation.
-
To keep the equipment dry, the use of heaters is required in some cases (for example, during seasonal or low periods of loading and equipment de-energization).
-
Consult the Engineer of Record for the appropriate environmental control settings or means to mitigate environmental influences.
-
If so equipped, ensure that the thermostats and/or humidistats are set to mitigate condensation. A minimum of 200 watts of heat per section is suggested.
-
If heaters are being used with the equipment that were not included in the equipment by Schneider Electric, they must be clean and free of debris and grease. Greasy and/or smoky heaters can contaminate electrical insulation and lead to dielectric breakdown and/or tracking.
-
-
Shipping packaging is not suitable for and cannot be used by itself for equipment storage unless otherwise indicated on the shipping packaging labeling.
-
When receiving equipment, the equipment may be at a lower temperature than the ambient air temperature. Allow time for the equipment temperature, including the temperature of internal components, to rise to ambient air temperatures before making openings in or otherwise or disturbing the packaging. Condensation can occur on and inside the equipment if warm air contacts cold surfaces of the equipment. Moisture damage can occur, destroying the dielectric capabilities of the equipment and rendering it unusable.
-
The factory shipping wrap around the equipment on shipping pallets is not suitable for non-enclosed over the road transportation that risks exposing the equipment to the elements. The factory shipping wrap around the equipment should remain on the equipment until the equipment is ready to be inspected and stored or inspected and installed. After receiving the equipment and allowing it to acclimate to the environment, remove the packaging and inspect the equipment for damage that may have occurred in transit. If damage is found or suspected, immediately file a claim with the carrier and notify the local Schneider Electric representative.
-
Follow these guidelines every time the equipment is moved to a new storage location or to its final destination.
Installation, Operation, and Maintenance Requirements
This equipment does not achieve its ratings until it is installed per record/as-built drawings, installed per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be operated in a climate controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment is not suitable for outdoor storage.
In some cases (such as seasonal electrical loading, de-energized equipment, and standby/alternate power sources), the heat generated by equipment loading is insufficient to prevent condensation and alternate heat sources are required. If environmental controls such as a thermostat or humidistat are used, ensure their settings are sufficient to mitigate condensation and remain operational at all times. Consult the Engineer of Record for the appropriate environmental control settings.
Exposure to Moisture, Chemicals, and Condensation
If liquids such as moisture, chemicals, and condensation contact the electronics, circuit breaker, fuses, bussing, or other electrical components, do not attempt to clean or repair the equipment as this may lead to unrepairable damage. If the equipment is energized, de-energize it. If equipment is not energized, do not energize it. Contact the Schneider Electric Customer Care Center at 888-778-2733.
General Storage Conditions
CAUTION |
|---|
|
INAPPROPRIATE STORAGE CONDITIONS
Failure to follow these instructions can result in injury or equipment damage.
|
To preserve all characteristics of the circuit breaker during prolonged periods of storage, store the circuit breaker:
-
indoors
-
in its original packaging
-
in clean, dry, corrosion-free conditions (including no condensation and recommended relative humidity levels)
-
sheltered from the sun and rain
-
at an ideal temperature of +70°F (+21°C) with maximum allowable temperatures of + 23°F (– 5°C) and + 104°F (+ 40°C)
NOTE: To ensure the circuit breaker functions properly, do not allow the ambient storage temperature to exceed these minimum or maximum limits.
Average Relative Humidity For Storage
| Ideal value | ≤ 75% |
| Measured over a 24-hour period | ≤ 95% |
| Measured over a 1-month period | ≤ 90% |
The maximum storage period is 12 months. Place the circuit breaker in its permanent location as soon as possible. If the circuit breaker will be used in switchgear employing space heaters, install it only after the heaters are operating. If the circuit breaker is stored:
-
between 6 and 12 months, perform a routine level maintenance to ensure a correct circuit breaker operation.
-
beyond 12 months, contact the local Schneider Electric Service representative for circuit breaker check-up.
Use care when uncrating and handling the circuit breaker. After unpacking, check the circuit breaker carefully for:
-
broken or damaged parts
-
condensation marks or droplets
-
visible degradation (color change, rust, deposits, etc.)
If any damage, degradation, or condensation marks or droplets are detected, do not install the circuit breaker and contact the local Schneider Electric representative.
The circuit breaker must be stored in the open (O OPEN) position with the charging springs discharged and the racking mechanism in the "test/disconnected" position.
Storage Arrangements
CAUTION |
|---|
|
heavy load stacking
Failure to follow these instructions can result in injury or equipment damage.
|
WARNING
CAUTION
DANGER
DANGER