Masterpact MTZ2/MTZ3 Device Identification
The Masterpact MTZ2/MTZ3 device can be identified in the following ways:
-
Faceplate label on device
-
QR code on the Micrologic X control unit
-
Identification labels on the device and on the cradle
-
Product identification label
-
Product checked label
-
Accessory voltages label
-
Faceplate Label
-
QR code
Masterpact MTZ2/MTZ3 Product Identification Label
|
Legend |
Description |
Explanation |
|---|---|---|
|
A |
Product code |
The product code represents the complete configuration of a Masterpact MTZ circuit breaker or switch. The product code:
|
|
B |
Schneider Electric internal identification number |
— |
|
C |
Description of device |
The following characteristics are specified:
|
|
D |
Certification Logos |
Logos of the mandatory certification of the device. |
|
E |
Device serial number |
— |
Masterpact MTZ2/MTZ3 Product Checked Label
Masterpact MTZ2/MTZ3 Accessory Side Label
Masterpact MTZ2/MTZ3 Faceplate Label
The faceplate label with the device information is located on the front cover of the device.
-
Device size and rated current x 100 A
-
Device type symbol
-
Type of device: circuit breaker or switch
-
Frame size
-
Frequency
-
Standard
-
Interrupting ratings
-
Temperature rating
-
Performance level
-
Place for IP address sticker
Masterpact MTZ2/MTZ3 QR Code
When the QR code on the front face of a Micrologic X control unit is scanned with a smartphone running a QR code reader and connected to the internet, the Go2SE landing page is displayed (see Go2SE Landing Page). The landing page displays information about the device and a list of menus.