Masterpact MTZ2/MTZ3 Drawout Device Racking
Masterpact MTZ2/MTZ3 Drawout Status
Masterpact MTZ2/MTZ3 Drawout Handling Conditions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Connection or disconnection of the drawout device requires insertion of the racking handle. When interlocks, padlocks, or an open door lock are in place, the racking handle cannot be inserted.
Masterpact MTZ2/MTZ3 Drawout Positions
The indicator located on the front of the cradle locally signals the position of the device in the cradle.
Masterpact MTZ2/MTZ3 Drawout Position Contacts
The position of the device in the cradle is indicated remotely by the position contacts:
-
CE: connected position
-
CT: test position
-
CD: disconnected position
The state of the position contacts changes according to the device position during racking-in and racking-out operations, as shown in the diagram below.
Masterpact MTZ2/MTZ3 Drawout Position Contact Without EIFE Ethernet Interface
Without an EIFE Ethernet interface, the standard configuration of the position contacts is:
-
3 CD disconnected position contacts
-
3 CE connected position contacts
-
3 CT test position contacts
The following optional configurations are available:
-
6 CE + 3 CT
-
3 CD + 6 CE
-
6 CD + 3 CE
-
9 CE
Masterpact MTZ2/MTZ3 Drawout Position Contacts with EIFE Ethernet Interface
With an EIFE Ethernet interface, the standard configuration of the position contacts is:
-
3 CD disconnected position contacts
-
3 CE connected position contacts
The following optional configurations are available:
-
3 CE + 3 CT
-
3 CD + 3 CT
-
6 CE
Masterpact MTZ2/MTZ3 Cradle Management Function
The cradle management function is used to:
-
Record and check the position of the moving part of the drawout device in the cradle.
-
Provide information about preventive maintenance actions.
-
Notify the remote controller about the position of the drawout device.
The cradle management function is performed by:
-
The EIFE Ethernet interface (refer to Enerlin’X IFE Ethernet Interface for One Circuit Breaker - User Guide (DOCA0084EN), available at the Schneider Electric website).
-
The IO module (refer to Enerlin’X IO Input/Output Application Module for One Circuit Breaker - User Guide (0613IB1317), available at the Schneider Electric website).
Masterpact MTZ2/MTZ3 Disconnection
Masterpact MTZ2/MTZ3 Drawout Handling Conditions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Connection or disconnection of the drawout device requires insertion of the racking handle. When interlocks, padlocks, or an open door lock are in place, the racking handle cannot be inserted.
Racking Out from Connected to Test Position
Racking Out from Test to Disconnected Position
Masterpact MTZ2/MTZ3 Connection
Masterpact MTZ2/MTZ3 Drawout Handling Conditions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Connection or disconnection of the drawout device requires insertion of the racking handle. When interlocks, padlocks, or an open door lock are in place, the racking handle cannot be inserted.
Racking-In from Disconnected to Test Position
Racking In from Test to Connected Position
Removing Masterpact MTZ2/MTZ3 Device from the Cradle
Masterpact MTZ2/MTZ3 Device Removal
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
The cradle must be securely fastened when installing or
removing the device.
Failure to follow these instructions can result in equipment damage.
|
Lifting the Masterpact MTZ2/MTZ3 Device
Both the device and cradle have a carrying grip for lifting. To lift, use an overhead lifting device attached to the carrying grip, following the directions given in this section.
DANGER |
|---|
|
Hazard of device falling
Failure to follow these instructions will result in death or serious injury.
|
Lift the device from the cradle rails by using the carrying grip located on the sides of the device.
Masterpact MTZ2/MTZ3 Circuit Breaker Weights
|
Frame Rating |
Connector Type* |
Weights (lbs./kg.) |
||||||||
|---|---|---|---|---|---|---|---|---|---|---|
|
Circuit Breaker |
Cradle |
Connector |
Pallet |
Total |
||||||
|
MTZ2 |
MTZ3 |
MTZ2 |
MTZ3 |
MTZ2 |
MTZ3 |
MTZ2 |
MTZ3 |
|||
|
800–2000 A, Drawout |
FCF |
109/50 |
142/65 |
97/44 |
116/53 |
42/19 |
55/25 |
17/8 |
265/121 |
330/151 |
|
FCT |
109/50 |
142/65 |
97/44 |
116/53 |
84/38 |
109/50 |
17/8 |
307/140 |
384/176 |
|
|
RCTH/RCTV |
109/50 |
142/65 |
97/44 |
116/53 |
17/8 |
22/10 |
17/8 |
240/110 |
297/136 |
|
|
800–2000 A, Fixed-Mounted |
FCF |
109/50 |
142/65 |
— |
— |
42/19 |
55/25 |
17/8 |
168/77 |
214/98 |
|
FCT |
109/50 |
142/65 |
— |
— |
84/38 |
109/50 |
17/8 |
210/96 |
268/123 |
|
|
RCTH/RCTV |
109/50 |
142/65 |
— |
— |
17/8 |
22/10 |
17/8 |
143/66 |
181/83 |
|
|
2500–3000 A, Drawout |
RCTH/RCTV |
127/58 |
165/75 |
124/57 |
149/68 |
26/12 |
34/15 |
17/8 |
294/135 |
365/166 |
|
FCT |
127/58 |
165/75 |
124/57 |
149/68 |
80/36 |
104/47 |
17/8 |
348/159 |
435/198 |
|
|
2500–3000 A, Fixed-Mounted |
FCT |
127/58 |
165/75 |
— |
— |
80/36 |
104/47 |
17/8 |
224/102 |
286/130 |
|
RCTH/RCTV |
127/58 |
165/75 |
— |
— |
26/12 |
34/15 |
17/8 |
170/78 |
216/98 |
|
|
2000 A L1/L1F & 3200 A, Drawout |
RCOV |
127/58 |
165/75 |
124/57 |
149/68 |
100/46 |
130/59 |
17/8 |
368/169 |
461/210 |
|
3200 A, Fixed-Mounted |
RCOV |
127/58 |
165/75 |
— |
— |
100/46 |
130/59 |
17/8 |
244/112 |
312/142 |
|
4000 A, Fixed-Mounted |
RCOV (Special) |
127/58 |
165/75 |
— |
— |
115/52 |
145/66 |
17/8 |
259/118 |
327/149 |
|
3200 A L1 & 4000 A, Drawout |
FCF |
227/103 |
295/134 |
278/126 |
334/152 |
84/38 |
109/50 |
39/18 |
628/285 |
777/354 |
|
FCT |
227/103 |
295/134 |
278/126 |
334/152 |
168/76 |
218/99 |
39/18 |
712/324 |
886/403 |
|
|
RCTH/RCTV |
227/103 |
295/134 |
278/126 |
334/152 |
52/24 |
68/31 |
39/18 |
596/271 |
736/335 |
|
|
4000 A, Fixed-Mounted |
RCTH/RCTV |
227/103 |
295/134 |
— |
— |
52/24 |
68/31 |
39/18 |
318/145 |
402/183 |
|
5000 A, Drawout |
FCT |
227/103 |
295/134 |
278/126 |
334/152 |
168/77 |
218/99 |
39/18 |
712/324 |
886/403 |
|
RCTH/RCTV |
227/103 |
295/134 |
278/126 |
334/152 |
52/24 |
68/31 |
39/18 |
596/271 |
736/335 |
|
|
5000 A, Fixed-Mounted |
RCTH/RCTV |
227/103 |
295/134 |
— |
— |
52/24 |
68/31 |
39/18 |
318/145 |
402/183 |
|
6000 A, Drawout |
RCTV |
227/103 |
295/134 |
278/126 |
334/152 |
396/180 |
528/240 |
39/18 |
940/427 |
1196/544 |
|
6000 A, Fixed-Mounted |
RCTV |
227/103 |
295/134 |
— |
— |
396/180 |
528/240 |
39/18 |
662/301 |
862/392 |
Installing Masterpact MTZ2/MTZ3 Device in the Cradle
Masterpact MTZ2/MTZ3 Drawout Handling Conditions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Connection or disconnection of the drawout device requires insertion of the racking handle. When interlocks, padlocks, or an open door lock are in place, the racking handle cannot be inserted.
Masterpact MTZ2/MTZ3 Optional Cradle Rejection Feature
The cradle rejection feature (see Masterpact MTZ2/MTZ3 Cradle Rejection Feature) allows the installation of a drawout device only in a cradle with compatible characteristics.
Installing Masterpact MTZ2/MTZ3 Devices in the Cradle
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGe
Failure to follow these instructions can result in equipment damage.
|
|
Step |
Action |
|
|---|---|---|
|
1 |
If the cradle is not installed in a switchboard or panelboard, securely fasten the cradle on a pallet. |
|
|
2 |
Inspect the circuit breaker clusters for missing or misaligned clusters. See the bulletin shipped with the circuit breaker for information on checking, installing, and lubricating clusters. |
|
|
3 |
Remove the racking handle from its storage space. |
|
|
4 |
Check that the cradle indicator is in the disconnected position: If the cradle indicator is not in the disconnected position, follow the steps on disconnecting the drawout device (see Masterpact MTZ2/MTZ3 Disconnection) . |
|
|
5 |
Press the rail release tabs. |
|
|
6 |
Pull out the drawout grips until the extension rails are fully extended. NOTE: The right-hand rail cannot be extended if the racking handle has not been removed. |
|
|
7 |
Install the device on the extension rails by using appropriate lifting equipment. Check that the slots on the device are correctly aligned with the guides on the rails while bringing the device down. |
|
|
8 |
Detach the lifting equipment. |
|
|
9 |
Check that the device is in the open position. |
|
|
10 |
Using both hands, push in the device so that the rails are inserted to the maximum in the cradle. Take care not to push the control unit. |
|
|
11 |
Check that the rail release tabs are in the correct position. Result: The device is in the disconnected position. |
|
DANGER
DANGER