Opening Masterpact MTZ Devices
Conditions Required to Open
To open the device, the device must be closed (I).
Opening the Masterpact MTZ2/MTZ3 Mechanism in All Control Modes
The device can be opened in the following ways in all control modes:
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
If the device does not open, refer toTroubleshooting.
Opening the Masterpact MTZ2/MTZ3 Mechanism in Auto Control Mode
In addition, the device can be opened in the following ways when Auto control mode is configured.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
|
Opening Type |
Control Mode |
Accessories |
Opening Action |
|---|---|---|---|
|
Through IO module |
Auto: Local or Auto: Remote |
Communicating shunt trip (MX diag&com) |
Open the device by using the predefined application 2 Breaker Operation of the IO module.
Refer to Enerlin’X IO Input/Output Application Module for One Circuit Breaker - User Guide (0613IB1317). |
|
ULP port |
|||
|
IO module |
|||
|
Through Ecoreach software |
Auto: Local |
Communicating shunt trip (MX diag&com) |
Send a command to open to the device from Ecoreach software running on a PC connected locally to the device through the mini USB port on the Micrologic X control unit. This opening action is password-protected. Refer to Ecoreach Online Help (DOCA0069EN). |
|
Through Masterpact MTZ Mobile App |
Auto: Local |
Communicating shunt trip (MX diag&com) |
Send a command to open to the device from the Masterpact MTZ Mobile App with Masterpact Operation Assistant Digital Module, through Bluetooth wireless communication or USB OTG connection. The opening action is password-protected. |
|
Masterpact Operation Assistant Digital Module |
|||
|
Through communication |
Auto: Remote |
Communicating shunt trip (MX diag&com) |
Send a command to open to the device through the communication network. This opening action is password-protected. Refer to Masterpact MTZ - Modbus Communication Guide (OCA0105EN). NOTE: Ecoreach software running on a PC connected to the device
through the communication network can be used to send commands to
open.
|
|
ULP port module |
|||
|
Communication interface |
|||
|
Through IFE/EIFE webpages |
Auto: Remote |
Communicating shunt trip (MX diag&com) |
Send a command to open to the device from the IFE/EIFE control webpage. This opening action is password-protected. Refer to: |
|
ULP port module |
|||
|
Communication interface |
If the device does not open, refer to Troubleshooting.
DANGER