Diagnosing Micrologic X Control Unit Alarms
Micrologic X Control Unit Diagnosis Sequence
The following table shows the sequence of actions to take after an alarm is detected by the Micrologic X control unit. Further explanation of each action is given in the following paragraphs.
|
Step |
Description |
|---|---|
|
1 |
Identify the alarm detected. |
|
2 |
Acknowledge the alarm cause on the Micrologic X display screen. |
|
3 |
Consult the list of alarms and perform the recommended actions. |
Identifying the Micrologic X Control Unit Alarm
The Micrologic X control unit indicates alarms with:
-
The ready LED (flashing green or off).
-
The service LED (red or orange).
-
A pop-up alarm screen (red or orange).
Two levels of alarm are detected and indicated by the color of the service LED:
-
Red for high-severity alarms.
-
Orange for medium-severity alarms.
|
Health Status LEDs |
Micrologic X Display Screen |
Trip Cause LEDs |
Probable Cause |
|---|---|---|---|
Ready LED flashing green. Service LED orange. |
All LEDs are off. |
Medium severity alarm (see Recommended Action after Detection of a Medium Severity Micrologic X Alarm). |
|
Service LED red. Ready LED flashing green. Service LED red. Ready LED off. |
All LEDs are off. All LEDs are on. |
High severity alarm (see Recommended Action after Detection of a High Severity Micrologic X Control Unit Alarm). |
Acknowledging the Alarm on the Micrologic X Display Screen
|
Step |
Action |
|---|---|
|
1 |
Press OK. The display screen displays:
|
|
2 |
Consult the list of alarm messages in the following tables and perform the actions recommended. |
|
3 |
Press OK to acknowledge the trip and return to the Home menu. |
|
4 |
Press the Test/Reset button for three seconds to reset the control unit and switch off the service LED. |
Recommended Action after Detection of a High Severity Micrologic X Control Unit Alarm
|
Code |
Alarm Message |
Alarm Description |
Recommended Action |
|---|---|---|---|
|
0x1400 |
CU self-test major malfunction |
The control unit self-test detected a major malfunction in the control unit operation. NOTE: The malfunction trips or does not trip the device, depending on how the fallback position is configured. The control unit self-test had invalid results. NOTE: The invalid self-test result trips or does not trip the device,
depending on how the fallback position is configured.
|
Call Schneider Electric field service to replace the control unit. |
|
0x1409 |
Unable to read sensor plug |
The control unit is unable to read the value of the sensor plug. |
Check connection of the sensor plug and performer plugs. If the connection is good but the control unit is still unable to reach the value, replace the sensor plug or the control unit. |
|
0x1413 |
Ig test - no trip |
The ground fault (Ig) test trip not executed. |
Restart the test. If it does not execute again, replace the control unit. |
|
0x1430 |
Protection reset to default setting if rebooted. |
If switched off, the control unit will be reset at next reboot to the default values of the protection settings. |
Call Schneider Electric field service to replace the control unit. |
|
0x1442 |
Contact wear > 100%. |
The contact wear indicator reached the threshold of 100%. |
Replace the circuit breaker. |
|
0x1444 |
CB has reached the max number of operations |
The circuit breaker reached the maximum number of operations. |
Replace the circuit breaker. |
|
0x1451 |
MCH has reached the max number of operations |
The spring charging motor (MCH) reached the maximum number of operations. |
Replace the MCH. |
Contact a Schneider Electric field service representative for more information about who can carry out the recommended actions.
Recommended Action after Detection of a Medium Severity Micrologic X Alarm
|
Code |
Alarm Message |
Alarm Description |
Recommended Action |
|---|---|---|---|
|
0x03F5 |
Ir prealarm (I > 90% Ir) |
The long time protection prealarm started: at least one of the phase or neutral currents is higher than 90% Ir threshold. The circuit breaker is operating close to Ir threshold. |
Check the load. |
|
0x0D00 |
Critical hardware modules discrepancy |
There is a major hardware discrepancy between the installed modules that prevent them from operating. |
In the Ecoreach
Firmware menu, see which module has the discrepancy. |
|
0x0D01 |
Critical firmware modules discrepancy |
There is a major software discrepancy between the installed ULP modules that prevent them from operating. |
With Ecoreach software, upgrade the firmware in the module . |
|
0x0D02 |
Non-critical hardware modules discrepancy |
There is a minor hardware discrepancy between the installed modules that prevent them from operating correctly. |
Plan to replace the module. |
|
0x0D03 |
Non-critical firmware modules discrepancy |
There is a minor software discrepancy between the installed modules that prevent them from operating correctly. |
With Ecoreach software, upgrade the firmware in the module. |
|
0x0D06 |
Config error IO/CU: dual settings or inhibit cls. |
There is a declaration discrepancy between the IO module and the control unit. |
Use Ecoreach software to correct the mismatch, as follows:
|
|
0x0D08 |
Address conflict between modules |
The control unit self-test detected the unexpected presence of IO2 module when IO1 is not present. |
Check the supply of the IO#1 module. |
|
0x0D09 |
Firmware discrepancy within control unit |
The control unit self-test detected a discrepancy between the firmware versions of control unit processors. |
Use Ecoreach software to upgrade the firmware in the control unit. |
|
0x0D0C |
Config mismatch IO/CU - optional protection inhibit |
There is a declaration discrepancy between the IO module and the control unit for inhibition of optional protection functions. |
Using Ecoreach software:
|
|
0x0D0D |
Config.error IO/CU- Local/Remote mode |
There is a declaration discrepancy between the IO module and the control unit for local/remote mode assignment. |
Using Ecoreach software:
|
|
0x101C |
Circuit breaker did not open or close |
The circuit breaker did not open or to close as expected. |
Visually check circuit breaker position and plan maintenance. |
|
0x1108 |
Protection changed by Bluetooth / USB / IFE |
The protection parameters were changed by communication through Modbus, Ecoreach, or the MTZ mobile app.. |
For information: No action is required. |
|
0x1120 |
Communication lost with IO#1 module |
The control unit lost communication with the IO#1 module |
Check the power supply of the IO#1 module. Check the ULP cable connection. |
|
0x1121 |
Communication lost with IO#2 module |
The control unit lost communication with the IO#2 module |
Check the power supply of the IO#2 module. Check the ULP cable connection. |
|
0x1122 |
Communication lost with EIFE or IFE module |
The control unit lost communication with the EIFE or IFE module |
Check the power supply of the IFE module. Check the ULP cable connection. |
|
0x1123 |
Communication lost with IFM module |
The control unit lost communication with the IFM module. |
Check the power supply of the IFM module. Check the ULP cable connection. |
|
0x112C |
Control unit firmware upgrade unsuccessful |
The firmware upgrade of the control unit was unsuccessful. |
Restart the upgrade procedure. If the message is displayed again, call Schneider Electric field service. |
|
0x1407 |
Control unit self test |
The control unit self-test had unexpected results. |
Plan to replace the control unit. |
|
0x140A |
Invalid display screen or wireless communication |
Control unit self-test detected an invalid result on display screen or the wireless module. |
Plan to replace the embedded display screen, which contains the wireless antenna. |
|
0x1411 |
Invalid measurement and optional protection |
Control unit self test detected an invalid result for metering and other protection |
Monitor the control unit. If other invalid self-test results occur, plan to replace the control unit. |
|
0x1412 |
NFC invalid communication |
The control unit self-test detected an invalid NFC communication |
Plan to replace the control unit. |
|
0x1422 |
Bluetooth communication lost |
The control unit self-test found no Bluetooth communication |
Plan to replace the control unit. |
|
0x1433 |
Replace battery |
The lithium battery is under 3 V and needs to be replaced soon. |
Replace the battery. |
|
0x1434 |
Self diagnostic test – firmware |
The control unit self-test detected a firmware internal problem. |
Use Ecoreach software to upgrade the firmware version of the control unit. |
|
0x1436 |
Control unit alarm reset |
The control unit self-test detected an invalid result in the control unit and corrected it. |
Monitor the control unit. If other self-test invalid results occur and are corrected, plan to replace the control unit. |
|
0x1437 |
Battery not detected |
The required battery is not present. |
Add battery. |
|
0x1438 |
Main voltage loss and circuit breaker is closed |
The circuit breaker is closed but no voltage is detected. |
Check main voltage. |
|
0x1440 |
Contact wear is above 60%. Check contacts. |
The contact wear indicator has reached or is above the threshold of 60%. |
Check contact wear. |
|
0x1441 |
Contact wear is above 95%. Plan for replacement. |
The contact wear indicator has reached or is above the threshold of 95%. |
Plan to replace the circuit breaker. |
|
0x1443 |
Less than 20% CB operation remaining |
The remaining number of operations of the circuit breaker is less than 20%. |
Plan to replace the circuit breaker. |
|
0x1450 |
MCH charging operations above threshold |
The number of operations of the spring charging motor (MCH) reached the alarm threshold. |
Plan to replace the MCH. |
|
0x1460 |
Invalid self test – MX1 shunt trip |
The control unit self-test detected an invalid result for the shunt trip (MX1). |
Replace the shunt trip (MX1). |
|
0x1461 |
MX1 shunt trip not detected. |
The control unit self-test detected the unexpected absence of the shunt trip (MX1). |
Check the connection of the shunt trip (MX1). |
|
0x1462 |
Invalid self test – XF shunt close |
The control unit self-test detected an invalid result for the shunt close (XF). |
Replace the shunt close (XF). |
|
0x1463 |
XF shunt close not detected. |
The control unit self-test detected the unexpected absence of the shunt close (XF). |
Check the connection of the shunt close (XF). |
|
0x1464 |
Invalid self test – MN undervoltage release |
The control unit self-test detected an invalid result for the undervoltage release (MN). |
Replace the undervoltage release (MN). |
|
0x1465 |
MN undervoltage release not detected |
The control unit cannot detect the undervoltage release (MN). |
Check the connection of the undervoltage release (MN). |
|
0x1466 |
Voltage loss on MN undervoltage release |
— |
Check the control voltage. |
|
0x1468 |
Invalid self test – MX2 shunt trip |
The control unit self-test detected an invalid result for the shunt trip (MX2). |
Replace the shunt trip (MX2). |
|
0x1469 |
MX2 shunt trip not detected |
The control unit cannot detect the shunt trip (MX2). |
Check the connection of the shunt trip (MX2). |
|
0x1474 |
Protection settings no longer accessible |
The control unit cannot access the protection settings. |
Call Schneider Electric field service to replace the control unit. |
|
0x1411 |
Invalid measurement and optional protection |
The control unit self-test detected an invalid result in the metering or optional protection functions of the control unit. |
Plan to replace the control unit. |
|
0x6200 |
Ir start (I > 105% Ir) |
The long time protection started: at least one of the phase or neutral currents is higher than the Ir threshold. The circuit breaker will trip at the end of the time delay. |
Operation information. No action required. |
|
0x6300 |
Ir operate |
The long time protection operated: at least one of the phase or neutral currents is higher than the Ir threshold and the time delay is elapsed. |
Reset the device (see Resetting Masterpact MTZ Devices) or use the Masterpact MTZ Mobile App Power restoration assistant. |
|
0x6301 |
Isd operate |
The short time protection operated: at least one of the phase or neutral currents is higher than the Isd threshold and the time delay is elapsed. |
Reset the device (see Resetting Masterpact MTZ Devices) or use the Masterpact MTZ Mobile App Power restoration assistant. |
|
0x6302 |
Ii operate |
The instantaneous protection operated: at least one of the phase or neutral currents is higher than the Ii threshold (no time delay). |
Reset the device (see Resetting Masterpact MTZ Devices) or use the Masterpact MTZ Mobile App Power restoration assistant. |
|
0x6303 |
Ig operate |
The ground-fault protection operated: the ground-fault current is higher than the Ig threshold and the time delay tg is elapsed. |
Reset the device (see Resetting Masterpact MTZ Devices) or use the Masterpact MTZ Mobile App Power restoration assistant. |
|
0x6306 |
Ultimate self-protection (SELLIM) operate |
The integrated instantaneous protection (SELLIM) operates: at least one of the phase or neutral currents is higher than the SELLIM threshold (no time delay). |
Reset the device (see Resetting Masterpact MTZ Devices) or use the Masterpact MTZ Mobile App Power restoration assistant. |
|
0x631D |
Ultimate self-protection trip (DIN/DINF) operate |
The integrated instantaneous protection (DIN/DINF) operates: at least one of the phase or neutral currents is higher than the DIN/DINF threshold (no time delay). |
Reset the device (see Resetting Masterpact MTZ Devices) or use the Masterpact MTZ Mobile App Power restoration assistant. |
Contact a Schneider Electric field service representative for more information about who can carry out the recommended actions.