Resetting the Circuit Breaker after a Trip Due to an Invalid Micrologic X Control Unit Self-Test
Masterpact MTZ Circuit Breaker Reset Sequence
The following table shows the sequence of actions to take after a trip. Further explanation of each action is given in the following paragraphs.
|
Step |
Description |
|---|---|
|
1 |
Identify the tripping cause. |
|
2 |
Acknowledge the trip message on the Micrologic X trip unit display screen. |
|
3 |
Consult the list of possible trip causes and perform the actions recommended to restart after the trip. |
|
4 |
Reset the circuit breaker (see Resetting Masterpact MTZ Devices). |
|
5 |
When the circuit breaker is ready-to-close, reclose it (see Closing the Masterpact MTZ2/MTZ3 Mechanism) |
Masterpact MTZ Circuit Breaker Trip Cause Identification
|
Status LEDs |
Micrologic X display screen T |
Trip Cause LEDs |
Probable Cause |
|---|---|---|---|
Ready LED off. Service LED red. |
All LEDs are on. |
Invalid Micrologic control unit self test (see Resetting the Circuit Breaker after a Trip Due to an Invalid Micrologic X Control Unit Self-Test). |
Micrologic X Display Screen Trip Message Acknowledgement
|
Step |
Action |
|---|---|
|
1 |
Press OK. The screen displays:
|
|
2 |
Consult the list of possible detected trip causes in the following table and perform the actions recommended. |
|
3 |
Press OK to acknowledge the trip and return to the Home menu. |
|
4 |
Press the Test/Reset button for 3 seconds to reset the control unit and switch off the trip cause and service LEDs. |
Recommended Actions After a Trip Due to Invalid Micrologic X Control Unit Self Test
|
Code |
Trip Message |
Description |
Recommended Action |
|---|---|---|---|
|
0x1400 0x1404 0x1405 0x1406 0x1416 |
CU self-test major malfunction |
The control unit self-test detected a major malfunction in the control unit operation. NOTE: The control unit may or may
not trip the circuit breaker, depending on how the fallback position
is configured.
|
Call Schneider Electric field service to replace the control unit. |
|
0x1402 |
Internal current sensor disconnected |
The control unit self-test detected the disconnection of an internal sensor of the circuit breaker. |
Call Schneider Electric field service to replace the control unit. |
|
0x1403 |
ENCT disconnected |
The control unit self-test detected the disconnection of the external neutral current sensor of the circuit breaker. |
Reconnect the external neutral current sensor (ENCT). |
|
0x6407 |
Self diagnostic trip |
The control unit tripped the circuit breaker for an unknown reason. |
Call Schneider Electric field service to replace the control unit. |