Masterpact MTZ2/MTZ3 Final Checks and Reporting
Masterpact MTZ Devices Final Checks
After completing the commissioning tests, check the following:
|
Step |
Action |
|---|---|
|
1 |
Check that connections are made with the correct tightening torque, that there are no tools or objects inside the equipment, and that all devices, doors, and protective covers are in position. |
|
2 |
Check that the device is off (open position) and the closing spring is charged. |
Project Report Generated by Ecoreach Software
Ecoreach software generates a project report with a list of the devices for that project. For each device it provides the following information:
-
The circuit breaker identification data.
-
The Micrologic X identification data, including the list of digital modules installed.
-
The list of accessories including internal accessories (for example, M2C programmable contacts), and external modules (for example, IO module).
-
The protection settings for the Micrologic X control unit.
-
The alarm settings.
-
The IFE, EIFE, or IFM communication interface settings.
Communication Test Report Generated by Ecoreach Software
Ecoreach software performs a communication test and generates a report of the test. For each device it provides the following information:
-
The name and type of the device.
-
The type of communication.
-
The address of the device or gateway.
-
The status of the connection.